Force Measurement Keeps UAVs Flying High

Unmanned Aerial Vehicles (UAVs) are revolutionizing various industries, from agriculture and entertainment to logistics and defense. UAVs, commonly known as drones, operate without a human pilot. A pilot controls them remotely on the ground or autonomously through pre-programmed flight plans or artificial intelligence.

UAVs have dramatically increased in popularity and applications across various sectors, revolutionizing industries and creating new opportunities for the use of these specialized aerospace vehicles. Current market estimates note there are more than 5 million units worldwide, which is estimated to grow to more than 7.5 billion in the next five years. The market size of UAVs for commercial, civil, and defense purposes is currently estimated to be valued at $30 billion today and will grow to $48 billion by 2028. In the US, the FAA currently has more than 785,000 registered drones, with more than half for commercial purposes.

There are various configurations of UAVs, each designed for specific tasks and environments.

  • Fixed-wing UAVs resemble traditional airplanes with wings and a fuselage. They offer long endurance, high speed, and efficient flight, making them ideal for surveillance, mapping, and long-range missions.
  • Rotary-wing UAVs, like helicopters and multi-rotors, are known for their vertical takeoff and landing capabilities, hovering, and maneuverability, making them suitable for aerial photography, inspections, and deliveries.
  • Hybrid UAVs combine features of both fixed-wing and rotary-wing designs, offering versatility and adaptability for various missions.

As this market expands, ensuring UAV performance, reliability, and safety becomes critical. Force measurement solutions are crucial in achieving these goals, offering engineers valuable insights during design, testing, and operation.

Force sensors, including load cells and multi-axis sensors, provide precise data on loads, stresses, and strains experienced by UAV components. To validate components and UAVs during flight, these sensors provide information that helps engineers optimize designs, validate structural integrity, and ensure airworthiness. Engineers can identify weaknesses in unmanned aerial vehicles by measuring forces during tests like wing fatigue, maneuverability, motor torque, fine-tuning control systems, and maximizing flight performance. Read more in our UAVs Solution Overview.

Forces can be monitored in flight using wireless sensors, enabling the detection of anomalies, overload conditions, or component failures, contributing to safer operations. Force data collected throughout the UAV lifecycle helps ensure compliance with industry regulations, maintain quality control, and support maintenance decisions.

Force Measurement Expanded Applications and Testing Use Cases

  • Advanced Material Testing
  • Wing Testing
  • Motor Torque Testing
  • Environmental Testing
  • Payload Integration and Delivery
  • Collision Avoidance Systems
  • Swarm Technology
  • Flight Control Systems
  • Simulators
  • Launch Validation
  • Structural Testing

UAVs have found applications across a broad spectrum of industries and sectors. In the civil domain, they are used for aerial photography, filmmaking, surveying, and search and rescue operations.

Commercially, UAVs have revolutionized agriculture, enabling precision farming, crop monitoring, and spraying. They are also used for infrastructure inspections, package delivery, and telecommunications.

In the defense sector, UAVs are used for surveillance, reconnaissance, target acquisition, and combat operations. As technology advances, the potential applications of UAVs are boundless, promising further innovation and transformation across various fields.

Drone Parcel Delivery Animated Application Note

Force measurement solutions are essential for driving innovation and ensuring the continued growth of the UAV market. By providing engineers with valuable data and insights, these technologies enable the development of safer, more reliable, and higher-performing UAVs for diverse applications. As the UAV industry continues to evolve, the role of force measurement solutions in pushing boundaries and achieving new heights will only become more critical.

UAV_InfographicPoster