Additive manufacturing, known as 3D printing, has developed and grown since its first prototypes for 3-dimensional printing in the 1980s. By the early 2000s, additive manufacturing was beginning to create functional products.
Today, additive manufacturing has improved and continues to expand in creating objects like small-scale models, prototypes, and even full-scale manufactured parts and products. Its popularity is driven by less process time and a much cheaper cost for production.
Additive manufacturing is a layer-by-layer process used to create objects, molds, or prototypes. Various materials, including polymers, metals, ceramics, foams, gels, and biomaterials, can be used. In contrast to traditional manufacturing, additive manufacturing can create complex shapes and small sizes. Interface load cells play a crucial role in this process, measuring the force or weight during dimensional printing to ensure precision and quality control.
Force Measurement Additive Manufacturing Applications
- Monitoring Nozzle Forces
- In-Situ Force Controls
- Tension and Compression Durability Tests
- Characterizing Mechanical Properties
- Calibrating Robotic Arms
- Material Yield, Strength, Stress and Strain Testing
- Equipment Maintenance Systems for Nozzle Blockage
- Machine Quality Checks
- Machining and Part Finishing
- Prosthetic Prototyping
- 4D Equipment Design
Sensor Technology Benefits in Additive Manufacturing Use Cases
Process Monitoring: Interface Mini load cells are used in additive manufacturing for process monitoring. These load cells can be integrated into 3D printers to monitor the forces exerted during printing. By measuring the force applied by the print head or the build platform, manufacturers can ensure that the printing process is proceeding as expected and detect any anomalies that may affect the quality of the final product.
Specification Quality Control: Load cells are ideal for verifying the mechanical properties of the printed parts. By subjecting the printed objects to controlled mechanical tests, such as tensile or compression tests, manufacturers can determine whether the parts meet the required specifications and standards.
Material Testing: Interface sensor technologies are commonly used to test the materials prior to the actual printing process. By measuring the forces required to extrude or deposit the material during the creation process. Manufacturers can evaluate the strength, flexibility, and viscosity of the material, thus achieving a consistent print quality.
Structural and Prototype Testing: Product designers and engineers use load cells and multi-axis sensors to gather critical measurement data in testing the final prototype or structure of objects being printed, ensuring structural integrity. Manufacturers can determine and assess different factors, such as stiffness, strength, and durability, of the prototype to ensure it meets the required performance criteria.
Interface offers a variety of sensors for use in additive manufacturing processes, including:
- LBM Compression Load Button Load Cells
- Load Pins
- LW General Purpose Load Washer Load Cells
- LWCF Clamping Force Load Cells
- S-Type Miniature Load Cells
- MB Miniature Beam Load Cell
- BMI Overload Protected Miniature Beam Load Cell
- MTFS Miniature Tension Force Load Cell
- REC Road End Load Cell
- ULC Ultra Low Capacity Load Cell
- WMC Sealed Stainless Steel Miniature Load Cell
The range of sensors is especially important for industries that need precision data and easy integration into equipment and testing. These include industries that are turning to additive manufacturing, such as aerospace, medical, and automotive. Selecting the right load cell is critical to product development, and manufacturers rely on Interface due to the accuracy and reliability of our solutions.
Recap of Precision Machine Building and Automation Webinar
/in Blog /by Jamie GlassInterface’s webinar, Powering Up Precision Machine Building and Automation explores the essential role of sensor technology in today’s industrial landscape. Learn about load cells, torque transducers, multi-axis sensors and instrumenation used testing machines, robotics, IIoT and automation. The recorded event captures key trends, tips, and applications valuable to machine builders, engineers, testing labs, and manufacturers.
Force Sensors Automate Safety Systems in Industrial Facilities
/in Blog /by Jamie GlassInterface force sensor technologies help modernize industrial facilities by providing valuable data to monitor and improve worker safety. Our load cells, torque transducers, and multi-axis sensors are used for overload protection, quality control systems, lockout and alarm systems, equipment monitoring, robot and cobot safety programs, maintenance alerts, and operator safety guides.
Force Makes the Circular Economy Go Around
/in Blog /by Jamie GlassInterface load cells and instrumentation are used in different facilities and resource manufacturing processes within the circular economy. Our sensor technologies help to measure and monitor forces, loads, and weight within the tools, robotics, and machinery used to optimize resources. Our sensors are also commonly used to test new products for material strength, fatigue lifecycle, quality, and function.
Strain Testing 101
/in 101 Series, Blog /by Jamie GlassInterface tension and compression load cells are used for strain testing across multiple industries. Learn about strain testing, a very common in general test and measurement applications. Strain refers to the deformation or shape a material experiences due to applied stress. Load cells are used to measure how much a sample or material stretches, compresses, or shears and distorts in response to a force.
The Convenience of Interface Portable Instrumentation Devices
/in Blog /by Jamie GlassInterface portable instrumentation devices allow measurements from load cells, torque transducers, and multi-axis sensors to be taken on-site, eliminating the need for a single testing location. Common use cases for portable devices are continuous monitoring applications. Additionally, portable instruments are user-friendly and require minimal setup, making them ideal for field applications or quick spot checks. Their compact size suits them for tight spaces or situations where benchtop instruments are impractical.
Powering Up Precision Machine Building and Automation Webinar
/in Virtual Event /by Jamie GlassInterface’s new webinar explores the world of load cells, torque transducers, multi-axis sensors, wireless technologies, and instrumentation used in machine building and automation. Get engineering tips on the latest advancements in sensor technology, including miniaturization, wireless integration, and the rise of the Industrial Internet of Things (IIoT). Join us to explore building smarter, more responsive machines.
Load Cells for Adhesive and Bonding Shear Testing
/in Blog /by Jamie GlassInterface provides load cells for adhesive and bond force testing. A shear testing machine uses a load cell to measure the shear strength of bonds and adhesives. A peel test is common for adhesives, adhesive-coated tapes, and paints. Load cells quantify the results and help to determine the failure of the paint and adhesive, an important quality control and design requirement.
The Textile Industry’s Future Demands Force Measurement Solutions
/in Blog /by Jamie GlassInterface force, torque, and weight measurement devices are valuable tools that can revolutionize the textile industry. By embracing this cutting-edge technology, manufacturers can unlock valuable process insights, enhance production for unparalleled efficiency, ensure consistency in fabric quality, extend equipment use, and significantly reduce maintenance costs.
Load Cells Elevate Gantry Crane Performance
/in Blog /by Jamie GlassInterface load cells, load pins, tension links, wireless telemetry systems, and instrumentation devices are used for gantry crane safety monitoring, alert systems, overloading protection, retrofitting old equipment, and accurately measuring the tension, force, and weight during lifting operations.
What is Proof Testing and Why Does it Matter?
/in Blog /by Jamie GlassInterface load cells and data acquisition systems are used for proof testing, which determines the strength and integrity of a test subject by applying a controlled, measured load to it. What is proof testing? Learn the steps of proof testing for stress, fatigue, and materials. It is frequently used by industries such as construction, natural resources, infrastructure, heavy machinery, and manufacturing to verify the strong point and durability of objects and structures.