Rigging Engineers Choose Interface Measurement Solutions
Interface supports rigging engineers who design, plan, and oversee the rigging of heavy loads by providing high accuracy measurement solutions. Rigging is the process of using ropes, chains, and other lifting equipment to move and position large objects.
Rigging engineers typically work in maritime, construction, manufacturing, entertainment and energy industries. Interface is also seeing a growing demand for sensor technologies used by rigging engineers that work in aerospace, both for aircraft and space vehicle manufacturers.
The use of load cells to measure the weight of heavy loads, such as cranes, ships, rockets, theater equipment and machinery is on the rise. Rigging engineers use the data from load cells, load pins, load shackles, and tension links to ensure that the loads are not overloaded and that the rigging systems are properly designed for each use case. This often requires pairing the high accuracy sensor with instrumentation. For versatility wireless telemetry systems are useful for rigging engineers.
These vital engineering positions are responsible for rigging up and down cranes, loading and unloading ships, or moving heavy equipment around a factory floor. Rigging engineers that design and plan rigging systems for lifting and transporting heavy loads across various industries rely on accurate measurement data. They often oversee the rigging of heavy loads, ensuring that it is done safely and efficiently. They inspect rigging equipment for wear and tear, and make repairs as needed while maintaining records of rigging operations. Sensors and instrumentation play an important role.
Load cells are an important tool for rigging engineers. They provide valuable information that can be used to ensure the safety of rigging operations, whether they are for mooring tension tests in the maritime industry or for lifting an aircraft for wind tunnel testing. Load cells can be used in a variety of ways by rigging engineers. For example, they can be used to:
- Monitor the weight of a load in real time. This information can be used to make sure that the load does not exceed the safe lifting capacity of the rigging system. Sensors are often integrated into conveyor systems, hoppers, and other equipment to measure the weight or force being exerted. These devices are often used in industries like mining, agriculture, and manufacturing.
- Create a load map. A load map is a visual representation of the weight distribution of a load. This information can be used to ensure that the load is evenly distributed, and that the rigging system is properly designed no matter the size of structure or component.
- Set overload limits. Overload limits are set to prevent the rigging system from being overloaded. If the weight of a load exceeds the overload limit, an alarm will sound, and the rigging system will be shut down.
- Record load data. Load data can be recorded and used to track the weight of loads over time. This information can be used to identify trends and patterns that may indicate a need for maintenance or repairs.
- Secure equipment. The information from force and weight sensors is critical when lifting and securing equipment, such as appartus used in the entertainment sector, from arial arts rigging to stage set-up.
Rigging engineers use load pins, load shackles, and tension links in a variety of applications to measure and monitor loads, weight and tensions in different lifting and rigging operations.
- Crane and Hoist Monitoring: Load pins, load shackles, and tension links are commonly used in cranes and hoists to measure the load being lifted. These devices can be integrated into the lifting mechanism to provide real-time load monitoring, ensuring that the load remains within safe working limits. Application examples: Gantry Crane Weighing and Crane Force Regulation App Note
- Heavy Lifting and Rigging: Load measurement technologies are used in heavy lifting and rigging operations to measure the tension in cables, ropes, and other lifting components. By monitoring the tension, rigging engineers can ensure that the load is evenly distributed, and that the lifting equipment is not overloaded. Application examples: Lifting Heavy Objects and Aircraft Lifting Equipment
- Load Testing: Sensors are utilized in load testing scenarios to assess the strength and performance of lifting equipment, such as cranes, hoists, and winches. These devices provide accurate load measurements during the testing process, helping engineers determine if the equipment meets the required safety standards. Application examples: Rescue Helicopter Hoist Test and Harness Durability Testing
- Offshore and Marine Applications: Due to the ruggedized designs of Interface load pins, load shackles, and tension links, we see extensive use in offshore and maritime operations. They are employed in various lifting and mooring applications, including lifting heavy equipment onto offshore platforms, measuring tension in mooring lines, and monitoring loads on anchor systems. Application examples: Mooring Line Tension Testing App Note and Maritime Measurement Solutions for Onshore and Submersible Applications
- Infrastructure and Civil Engineering Projects: Load cells, load pins, load shackles, and tension links are actively used in construction and civil engineering projects for load monitoring purposes. They can be used in applications such as measuring loads on temporary structures, monitoring tension in cables and suspension systems, and ensuring safe load distribution during construction operations. Application examples: Power Line Tension Testing and Monitoring the Seismic Force of a Suspension Bridge
In all these applications, rigging engineers are using crucial data about loads, tensions, and forces, to ensure safety, optimize performance, and prevent equipment failures.
Load cells and measurement solutions can help to prevent overloading of rigging systems, which can lead to accidents and injuries. Accurate sensors help to improve the efficiency of rigging operations by providing real-time weight data. This information can be used to adjust the rigging system as needed, which can help to reduce the amount of time and effort required to lift and transport heavy loads.
Learn more about Interface’s Lifting Solutions and Weighing Solutions for Rigging Engineers with these resources:
WTS Yacht Rigging Inspection App Note
Bridge Construction Wind Monitoring