Tag Archive for: rigging

Untethered Precision with Wireless Complete Measurement Systems
Interface Wireless Complete Systems eliminate unknown parameters and configuration guesswork when pairing sensors with wireless telemetry devices. The versatility of paired wireless sensors and instrumentation supports applications where physical cables are either hazardous, impractical, or physically impossible to route. Interface's wireless calibrated complete systems are designed for easy deployment.

Understanding Dual Shear Load Cells
Interface dual shear load cells are strain gage sensors supported at both ends, with the force applied directly at the center of the beam. A double-ended shear beam load cell design is used in the high-performing Interface LowProfiles and load pins. The dual-ended design distributes force symmetrically across two matched shear webs. Strain gages are bonded to the machined webs inside the beam and configured in a full Wheatstone bridge circuit to convert mechanical shear stress into an electrical mV/V signal.

What Is the Difference Between Fatigue and Impact Testing?
Interface Tech Talk details why fatigue testing and impact testing are fundamentally different mechanical test methodologies that impose separate physical and electronic demands on measurement hardware. Learn about application differences, load cell and sensor selection, and instrumentation requirements for each type of test.

Transducers for Aircraft Ground Support Equipment Design and Operations
Accurate measurement of force and torque transforms ground support from reactive repairs to proactive, condition-based lifecycle management. Whether installing new hardware or upgrading existing equipment with direct-fit load pins, tension links, and load cells, continuous force, torque, and weight monitoring safeguards aircraft and ground personnel from unnoticed structural stresses, equipment failures, and overloading.

The Mechanics of Suspended Loads in Heavy Rigging
Interface products provide real-time measurements of cable tension and load weight to prevent dangerous overloads of rigging equipment. Rigging converts rotational, linear, or gravitational forces into controlled mechanical displacement. It relies on calculating vector forces, tension distribution, centers of gravity, and safe working load (SWL) limits to ensure that heavy components remain structurally stable and balanced throughout dynamic motion.

Engineering Thrills Using Sensor Technologies for Theme Parks and Venues
Interface provides entertainment venues, thrill ride engineers, and theme park attraction manufacturers with measurement solutions for complex mechanical systems, enabling them to create immersive guest experiences while meeting strict safety requirements. From roller coasters and motion platforms to automated stages and animatronic characters, engineers depend on precise force, torque, and weight measurements to ensure attractions operate safely and reliably.

Engineering Performance and Safety in Sports Equipment
Interface force measurement sensors allow engineers to push the limits of physics in sporting equipment design and testing. Sports technology use Interface high-accuracy load cells to provide the empirical evidence needed to innovate safely, ensuring that equipment is lighter, faster, and more resilient for professional and casual sports of all types.

Sensors Provide Intelligence for Safe and Automated Hoisting
Integrating Interface load cells, load pins, tension load links, and load shackles into hoisting equipment provides real-time force and weight data. Measurement sensors provide accurate data for overload protection, WLL, load balancing, alarm systems, weighing, equipment monitoring, and testing. Smart hoisting and automation utilizing sensors increase safety, ensure compliance, and prevent catastrophic failure.

Tension Load Link Systems and Applications
Interface tension link load cells are specialized force sensors designed to measure tensile or "pulling" forces. Tension load links are frequently used in demanding environments, including nearshore and offshore areas, which require certifications for hazardous locations. They're designed for lifting, weighing, mooring, towing, as well as tension testing and monitoring applications, and are used in marine, aerospace, manufacturing, construction, and logistics industries.