Tag Archive for: industrial automation

Refining Robotic Gripper Performance
High-resolution sensors are needed for greater precision and responsiveness in the design, testing, and monitoring of grippers used in robotics and industrial automation. Force sensing is essential for safe human interaction and for handling fragile tasks. Grippers in humanoids, collaborative robots, and robotic arm integrations that require compact, high-accuracy measurements use Interface load cells, mini load buttons, and multi-axis sensors.

Cycle Testing 101
Interface 101 series highlights cycle testing, which uses load cells, torque transducers, and multi-axis sensors to evaluate functional reliability, kinematic wear, seal integrity, switch actuation life, joint loosening, and mechanical degradation across hundreds, thousands, or millions of operating cycles. Cycle testing is an evaluation methodology used to verify product endurance, track mechanical wear, and establish operational life expectancy under repetitive dynamic loading.

Improving Manufacturing Logistics Using Precise Measurements
Interface sensor technologies integrate real-time force, tension, weight, and torque data into daily logistics operations, providing manufacturers with the visibility needed to eliminate bottlenecks, protect expensive handling machinery, and maintain the continuous throughput required in modern fulfillment. Precise measurements between mechanical equipment and digital warehouse controls drive efficiency and operational improvements across the factory.

LowProfile Complete Systems for Immediate Force Measurement Deployment
Interface LowProfile Load Cell Complete Systems are pre-configured measurement solutions to eliminate trial-and-error in setup by pairing the sensor with instrumentation, accessories, and software. System level calibration provides documented traceability across the entire signal path using the LowProfile and system components.

5-Axis Load Cells 101
An Interface 5-axis load cell is a multi-axis sensor designed to resolve complex multi-directional loading into three orthogonal forces and two bending moments (Fx, Fy, Fz, Mx, and My). By combining multiple sensing elements into one precisely machined structure, a 5-axis load cell provides comprehensive measurement of complex loading conditions that conventional single-axis load cells cannot accurately capture. Learn more in 5-Axis Load Cell 101, part of Interface's 101 Series.

2027 International Sales Meeting
Interface's exclusive ForceLeaders Summit will take place on August 20, 2026, in Pittsburgh, Pennsylvania. Join us for an advanced technical workshop on test and measurement. Topics include new load cells, instrumentation, best practices, complete systems, testing tools, sensor use cases, and valuable tips. Our force measurement seminars bring together experts and engineers working on projects across industries, including robotics, rockets, aircraft, manufacturing, industrial automation, energy, medical devices, and general testing programs. Together, we will discuss load cells, torque transducers, calibration, systems, applications, advancements in digital and wireless technologies, and multi-axis sensors. Most importantly, we will answer your questions. These are fast-paced, technical, hands-on events. Registration is required; seating is limited.

Mastering The Signal Chain in Test and Measurement
In test and measurement, Interface defines the signal chain as the interconnected hardware and software continuum that converts a physical event into validated engineering units. It encompasses the raw strain gage bridge from a load cell, regulated excitation sources, local analog conditioning, filtering, high-resolution digitization, network transmission, and the final analytical software interface. Learn engineering tips, application highlights, and why modern test and measurement requires planning for the entire signal chain to preserve data integrity.

Digital Twins Bridge Physical Stresses and Virtual Models in Test and Measurement
Interface sensor technologies are used in digital twins for structural testing, fatigue monitoring, and model validation. A digital twin uses force or torque inputs of load, torque, and weight to bind virtual simulations to actual mechanical behavior. By integrating Interface load cells, torque transducers, wireless telemetry systems, and digital instrumentation into your digital twin framework, you eliminate simulation drift and ground your virtual assets in real physical evidence.

How Sensor Technologies Advance Oil and Gas Robotics and Automation
Interface sensor technologies for oil and gas robotics test mobility, assess mechanical performance, and confirm the structural integrity of inspection tools. Robotics and automation in the oil and gas sector use load cells, torque transducers, and multi-axis sensors for infrastructure, production, maintenance, security, monitoring, and safety.