7 search results for:

IQ Blog

Demystifying Specifications Webinar

Interface's technical force measurement webinar Demystifying Specifications details descriptions, terms, values and parameters found in product datasheets for load cells, torque transducers, instrumentation and specialty products. Learn from our experts what specifications need critical review, recommendations based on product categories, and the insider point of view on what is most important in terms of specifications for different use cases and tests.

IQ Blog

Demystifying Specifications Webinar Recap

Interface's Demystifying Specifications recorded webinar details product specification basics, key values, terms to know, how to read a datasheet, what specs matter most in force measurement, and commonly asked questions. For Interface, specifications are detailed descriptions that outline the characteristics, features, and qualities of our products, systems, or services. Throughout the webinar, Interface experts provide tips on what to consider for high-speed, durability, precision and speciality load cell, torque transducer, multi-axis sensor and instrumentation product requirements.

IQ Blog

Why Is Load Cell Zero Balance Important to Accuracy?

Load cell zero balance is the signal of the load cell in the no-load condition. It is defined as the output signal of the load cell with rated excitation and no load applied. It refers to the amount of deviation in output between true zero and an actual load cell with zero load. It is usually expressed in the percentage of rated output (%RO). Zero balance is a test that can be done to understand calibration on a load cell.

IQ Blog

Load Cell Test Protocols and Calibrations

Load cells are conditioned in either tension or compression mode and then calibrated. For test protocols and calibration define the testing mode first. More tips from the Interface Load Cell Field Guide

IQ Blog

Load Cell Basics Sensor Specifications

Sensor specifications determine the accuracy of load cells. The sensor specifications relate to the max error of various parameters. Load cell basics from Interface.

IQ Blog

Specifying Accuracy Requirements When Selecting Load Cells

Interface load cells have detailed specification datasheets that outline accuracy and performance factors by model and capacity including nonlinearity, hysteresis, nonrepeatability, static error band and more.

IQ Blog

Considerations for Steel, Stainless Steel and Aluminum Load Cells

Three most used materials for load cells are aluminum, steel and stainless steel. Interface Chief Engineer Ken Vining helps you compare the material factors for comparing the best option based on testing requirements and use case.