INDUSTRIES: AUTOMOTIVE AND VEHICLE / ENERGY
SUMMARY |
Customer Need / Challenge
A rail station owner wanted to collect data on the load profiles for railcars as they were entering into the station in-motion. The customer wanted to build their own low cost set-up using components from Interface Inc. and their existing PC setup for the purpose of logging weight load characteristics in order to diagnose possible side to side loading issues, overload issues, wheel flats or wheel impact issues, at any railcar speed.
Interface Solution
12 Model 2400 50K capacity standard stainless steel load cells were mounted in to metal fabricated box-like structures and bolted into 6 consecutive cement rail ties, 1 on each side of each tie under the rail with a direct line of force with the rail. The cells were split into three groups of four: front, middle, and back. Each group of cells was connected to a dedicated BSC4 that accepted four load cell inputs. The BSC4s were connected to a PC through a USB hub.
Results
After all the connections were made the operator had a valuable tool for monitoring load characteristics which were used to detect a number of diagnostic conditions. The manager saved cost by creating his own set-up in-house for in-motion railcar load measuring as compared to alternative solutions/ proposals from other competitors.
MATERIALS |
Interface Products
- 12 x Model 2400 50K capacity Standard Stainless Steel Load Cell
- 3 x Model BSC4-USB Multi-Channel Bridge Amplifier & PC Interface Module
Alternative Setup
- 3 x Model JB104SS Stainless Steel Junction Box
- 3 x Model 480 Bidirectional Weight Indicator
- The load cells within the installed fixtures were connected via cables to the appropriate Model JB104SS Stainless Steel Junction Box, using proper protective accessories and maintaining clearance from any potential snag or crush points.
- Each junction box was then connected to its dedicated Model 480 Bidirectional Weight Indicator.
- After the set-up was complete the operator had full access to live load data from all 3 junction boxes which was used to diagnose railcar issues.
Additional Materials
- Customer Mounting Fixtures
- USB Hub
HOW IT WORKS |
- The customer made a special fixture that allowed for the mounting of the Model 2400 50K Capacity Standard Stainless Steel Load Cell. On the top there was a plate with a threaded rod which threaded into the load cell and on the bottom was an encasement that ensured proper clearance, stability, and proper enclosure from the elements.
- The cement rail ties were modified on both sides underneath the rail area to provide a recessed clearance for the cell fixtures. The fixtures were then fastened into the tie. Each tie has 2 fixtures. There were 6 ties altogether. There were 2 ties (4 cells) per group: front, middle, and back.
- The load cells within the installed fixtures were connected via cables to the appropriate BSC4-USB Multi-Channel Bridge Amplifier & PC Interface Module, using proper protective accessories and maintaining clearance from any potential snag or crush points.
- The interface modules were each connected to a PC through a USB hub.
- The PC had the software installed that came with the interface modules.
- After the set-up was complete the operator had full access to logged load data from all 12 load cells which was used to diagnose railcar issues.