Tag Archive for: metrology

Advantages and Selection of Stainless Steel Load Cells
Interface offers more than 50 stainless steel load cell models, with varying geometries and measurement capacities, built for extreme durability, hermetic protection, and accuracy. Discover the benefits, engineering advantages, key selection considerations, and applications of Interface stainless steel load cells.

How Do Universal Testing Machines Use Load Cells?
Universal testing machines (UTMs) are essential for material qualification, structural research, and quality assurance. Interface load cells sit directly in series with the moving crosshead and the upper specimen grip of a UTM. A machine controller reads the load cell continuously within a closed feedback loop to regulate crosshead travel, maintain constant loading rates, or hold targeted force thresholds during stress relaxation evaluations. The transducer measures the specimen resistance as it deforms. The data acquisition system pairs this instantaneous force data with displacement data to measure elasticity, yield point, and ultimate tensile strength.

2027 International Sales Meeting
Interface's exclusive ForceLeaders Summit will take place on August 20, 2026, in Pittsburgh, Pennsylvania. Join us for an advanced technical workshop on test and measurement. Topics include new load cells, instrumentation, best practices, complete systems, testing tools, sensor use cases, and valuable tips. Our force measurement seminars bring together experts and engineers working on projects across industries, including robotics, rockets, aircraft, manufacturing, industrial automation, energy, medical devices, and general testing programs. Together, we will discuss load cells, torque transducers, calibration, systems, applications, advancements in digital and wireless technologies, and multi-axis sensors. Most importantly, we will answer your questions. These are fast-paced, technical, hands-on events. Registration is required; seating is limited.

Addressing Technical FAQs in Torque Measurement
Interface answers advanced technical questions related to torque transducers and torque measurement. Explore the top 17 FAQs related to technicalities of torque measurement covering reaction vs rotary transducers, capacity selection, mounting alignments, couplings, calibration and metrology.

High-Fidelity 101
Interface 101 series details high-fidelity (Hi-Fi), a term referencing how accurately a measurement system reproduces the characteristics of a physical input. Load cell users may require a high-fidelity system where the digital output precisely reflects the mechanical force applied to the sensor. This integrity must be maintained throughout the entire signal chain, from the physical deformation of the strain gage to the final data output. Hi-Fi is very important in aerospace, additive manufacturing, and product efficiency such as lightweighting.

Bias and Variance for Benchmarking Outcomes in Force Measurement
In load cell selection, understanding the relationship between bias and variance is defined by sensor specifications. Interface details how these engineering concepts dictate performance, improve design, and optimize benchmarking outcomes using force measurement systems.

Why is Metrology Fundamental to Test and Measurement?
Metrology, the science of measurement, is the foundational pillar of the test and measurement industry. Metrology is critical for quality control, regulatory compliance, and the development of new products and processes across a wide range of industries. Interface LowProfile Load Cells and Gold Standard Calibration Solutions are standards of measurement excellence required in metrology.

Resistance Output Versus Rated Output
Rated Output (RO) is the dynamic electrical signal that directly represents the applied mechanical force. Resistance Output is a static electrical characteristic of the load cell's internal circuitry. When you are performing force measurements, you are primarily interested in the Rated Output. This value, in conjunction with your excitation voltage, enables you to accurately convert the measured millivolt signal into engineering units of force in lbf or Newtons. Discover how load cells work at the ultimate force measurement resource hub, Interface ForceEDU.

Strain Gage Interconnection to Bridge Configurations for Load Cells
Interface strain gages are fundamental to load cell technology. In forming quarter, half, or full bridges, the interconnection of strain gages in a Wheatstone bridge is a critical design choice that impacts performance, cost, and application suitability. Interface details this technical topic to answer key questions about load cell design and strain gages.