9 search results for:

IQ Blog

How Does Tensile Testing Work?

Interface supplies load cells for tensile testing. Tensile testing is fundamental in test and measurement. Load cells are commonly used in tension testing to measure and record the force or load applied to a specimen during the test. Tensile testing is used by researchers, testing labs, and engineers across industries including infrastructure, medical, manufacturing, aerospace, consumer goods, automotive, energy, and construction to measure stress, strain, elacity, fatigue and failure.

IQ Blog

Load Cells for Adhesive and Bonding Shear Testing

Interface provides load cells for adhesive and bond force testing. A shear testing machine uses a load cell to measure the shear strength of bonds and adhesives. A peel test is common for adhesives, adhesive-coated tapes, and paints. Load cells quantify the results and help to determine the failure of the paint and adhesive, an important quality control and design requirement.

IQ Blog

What is Proof Testing and Why Does it Matter?

Interface load cells and data acquisition systems are used for proof testing, which determines the strength and integrity of a test subject by applying a controlled, measured load to it. What is proof testing? Learn the steps of proof testing for stress, fatigue, and materials. It is frequently used by industries such as construction, natural resources, infrastructure, heavy machinery, and manufacturing to verify the strong point and durability of objects and structures.

IQ Blog

Wireless Telemetry Systems 101

Interface offers a wide range of wireless telemetry products including load cells, transmitters, bases, communication modules and data acquisition systems. A wireless telemetry system enables the remote measurement and transmission of data from one location to another without the need for physical wired connections.  Components in wireless telemetry systems typically include sensors, transducers, instrumentation, communication modules, transmitters, displays and printers. Learn more about Interface WTS products in our Wireless Telemetry Systems 101 overview.

IQ Blog

Are Load Cells Used in Vacuum Environments?

Interface provides load cells thare can be used in a vacuum environment. However, not all load cells are created equal or suited for this specialized use case. Vacuum testing labs are used by a variety of industries, including aerospace, medical, and defense. These labs are common for material process testing and used in R&D. Vacuum testing helps to identify potential problems with products and materials before they are used in a vacuum environment. Using quality load cells that are manufactured by force measurement experts in sensor technologies and experienced in working with vacuum testing labs and experts is an important consideration.

IQ Blog

What are IO-Link Load Cells

IO-Link can be used with load cells in industrial applications to enable enhanced monitoring, control, and diagnostics. Interface offers customization of our most popular load cells with IO-Link capabilities.

IQ Blog

What is Static Error Band Output?

Interface Tech Talk answers the question of what is static error band output. SEB is a band encompassing all points on the ascending and descending curves centered on the best-fit straight line. It is expressed in units of %FS. SEB Output at capacity is based on the best fit straight line. Learn how to calculate SEB, the benefits, and an engineering perspective on why SEB output is preferred over terminal output.

IQ Blog

Understanding the Anatomy of Fatigue Failure

Interface fatigue-rated load cells are designed to meet the demands of fatigue testing. As load cells are structural devices stressed during their normal use, they are commonly given ultimate overload ratings to characterize the magnitude of static load they will withstand without failing structurally. Learn more about fatigue theory from Interface force measurement experts.

IQ Blog

What is Moment Compensation?

Every Interface LowProfile load cell is moment compensated to minimize sensitivity to extraneous loads. Moment compensated load cells are designed to counteract the external forces or moments by using a configuration of strain gages and electronics that can detect and compensate for these forces. The strain gages are arranged in a way that allows the load cell to measure the force applied to it in multiple directions, and the electronics can then use this information to calculate the impact of external forces and moments on the measurement.