Tag Archive for: consumer products

Refining Robotic Gripper Performance
High-resolution sensors are needed for greater precision and responsiveness in the design, testing, and monitoring of grippers used in robotics and industrial automation. Force sensing is essential for safe human interaction and for handling fragile tasks. Grippers in humanoids, collaborative robots, and robotic arm integrations that require compact, high-accuracy measurements use Interface load cells, mini load buttons, and multi-axis sensors.

Sensor-Enablement for Household and Commercial Appliances
Interface equips appliance makers worldwide to design safer hardware, optimize resource efficiency, and deliver dependable performance to every consumer. Test and measurement throughout the household and commercial appliances lifecycle rely on load cells, torque transducers, and multi-axis sensors during the first proof of concept. Lab engineers conduct verification testing using sensors, and factory line production and assembly adopt transducers to improve operations. Manufacturers integrate sensor-enabled feedback systems to improve the user experience and reliability of the appliance.

Impact Testing for Millisecond Assessments
Interface impact testing force measurement solutions are used in material, component, and product tests, from sports equipment to autos and aircraft. High-velocity impact testing demands high-velocity sensors and low-latency instrumentation to capture millisecond-long force spikes without data gaps or signal clipping. Pairing the load cell and instrument is critical for a successful impact testing system.

Engineering Performance and Safety in Sports Equipment
Interface force measurement sensors allow engineers to push the limits of physics in sporting equipment design and testing. Sports technology use Interface high-accuracy load cells to provide the empirical evidence needed to innovate safely, ensuring that equipment is lighter, faster, and more resilient for professional and casual sports of all types.

The Consumable Continuum Demands Measurement Technology
Interface is a supplier of measurement solutions for the consumable continuum, which represents the entire lifecycle of a product, from the arrival of raw bulk materials to the moment a consumer opens the package. In high-volume production environments, force, torque, and weight measurement accuracy is the primary factor in determining the difference between a profitable run and a costly recall.

Esports Are Transforming Fundamental Gaming Hardware Performance
Esports is driving advancements in high-precision hardware design and testing using load cell technologies. Interface force measurement solutions for esports hardware, from controllers to simulators, are necessary for meeting the competitive requirements of elite performance, tactile consistency, and arena safety.

Lightweighting for Efficiency Demands Force Measurement
Interface details the connection in lightweight design, material behavior, and high-fidelity load data. Precise force measurement using load cells and instrumentation is foundational to lightweighting, ensuring it is quantifiable and verifiable. Interface sensor technologies enable engineers and designers to successfully push performance boundaries while ensuring the safety and reliability of components, products, and systems.

Engineering the Human Touch by Measuring Haptics
Using high-accuracy load cells enables designers to measure these haptic interactions during prototyping, ensuring the final product mimics the weight, snap, and texture of the real world. Interface provides measurement sensors and high-speed instrumentation needed to capture these micro-interactions and turn them into usable haptic data.

Raw Signals to Intelligent Force Sensing
Interface load cells, multi-axis sensors, and data acquisition systems are providing data for integrating artificial intelligence into force measurement systems. This represents a significant leap forward in precision, responsiveness, and reliability for these data use cases. The rise in use of strain gage outputs for AI is on the rise. The quality of the sensor is critical for these applications, and this is why Interface products are valuable for advanced analytics.