Tag Archive for: AxialTQ

Dynamic Versus Static Torque 101
Understanding the difference between dynamic and static torque is vital in selecting the right torque sensor. Dynamic (rotary) torque measurement is required when the sensor must rotate with the shaft, typically when the component operates at high speeds and/or undergoes significant angular acceleration. The sensor measures the applied or transmitted torque through the rotating shaft. Static (reaction) torque measurement occurs when there is no or negligible angular acceleration of the rotating element, or more commonly, when the measurement is taken on the non-rotating reaction element of a system.

Contact Resonance 101
Contact resonance can significantly damage measurement accuracy and even cause system failure. Interface 101 Series details how inherent mechanical clearances within the measurement system can turn harmless transient forces into potentially destructive oscillations. Contact resonance is a form of self-excited oscillation that occurs in mechanical systems involving mass, stiffness, and a clearance. Interface Load Cells 301 Characteristics and Applications Guide covers this important topic.

Accelerating Advanced Automotive Testing Using Torque Transducers
Interface rotary and reaction torque transducers are selected for Automotive testing applications due to their accuracy, durability, capacity, and capabilities. Advanced torque transducers drive innovation and facilitate the transition from concept to production in the auto industry shift toward increasing motor performance, fuel-efficient designs, Electric Vehicles (EVs), advanced safety systems, and the integration of Autonomous Vehicle (AV) technologies.

Torque Transducers Review Plus Glossary of Torque Terms
Interface torque transducers measure the twisting force or moment applied to an object. Review our torque glossary, engineering tips, and fundamentals about torque measurement, including a review from Interface's popular Torque 101 webinar.

Interface Measurement Solutions for Industry Testing Labs
Interface provides load cells, torque transducers, and instrumentation to automotive, aerospace, infrastructure, and medical device industry testing labs. Selecting standard equipment for a force measurement testing lab involves more than choosing the right transducer. Consider the entire testing ecosystem, including evaluating the mechanical connections, application, cycle counts, calibration standards, and environment.

Rotary Torque 101
Torque is the rotational force that causes an object to turn. Interface rotary torque transducers are versatile sensors that integrate electronics directly onto the rotating shaft. Engineers measure torque using torque transducers that convert a torsional mechanical input into an electrical output signal, typically a voltage or current. Rotary torque transducers are ideal for dynamic applications where continuous rotation is required, eliminating the need for complex wiring and reducing potential points of failure. They are commonly used in measuring torque for engines, gearboxes, robotics, aircraft, medical devices, tractors, and windmills. If it turns, it needs to be measured.

The Future of Automotive Performance Requires Precise Torque Measurement
Interface torque transducers have a driving impact on the automotive industry. Torque sensors transform how automotive engineers design, test, and manufacture vehicles, leading to new inventions and improvements in driving dynamics and production. Interface torque transducers are used in testing brakes, powertrains, electric motors, batteries, fuel pumps and other critical performance and safety components.

Interface Primer Dives Deep into Torque Measurement
Interface Torque Measurement Primer provides a comprehensive technical guide to navigate types of transducers, measurement calculations, intallation methods, accessories, mechanical considerations and environmental factors. Torque measurement can be simple or complex, and choosing the suitable transducer requires a deep understanding of your application’s needs. Torque Primer Review Part 2

Engineering Peak Performance in Auto Racing Requires Precision Measurement
Interface load cells and torque transducers provide precision measurements in auto racing vehicle design, testing, and performance tracking. The data acquired through these sensors, like the AxialTQ, helps performance auto engineers optimize vehicle components, ensuring they perform at their best under the intense conditions of a race.