Beyond the Obvious Forces of Product Testing

When most of us hear “product testing,” we picture a straightforward process: apply a force, measure the result, and see if the object passes or fails. But in the high-stakes world of professional testing labs, where everything from aerospace components to medical devices is validated, this simple picture dangerously ignores the realities of the work. Here, success isn’t just about applying force correctly. It is about anticipating, controlling, and understanding all the subtle, invisible forces that can derail a test, destroy expensive equipment, and compromise safety.

Experts who spend their lives methodically breaking things for a living know that the most critical factors are often the ones we never think about. These aren’t just theories. Product testing relies upon proven science and principles shared by engineers at Interface, a company that has spent decades instrumenting the world’s most demanding test labs.

We understand that a test isn’t just a procedure, but a complex system where the environment, the setup, and even the potential for catastrophe must be managed with extreme precision. This article reveals five surprising truths from these experts that will change how you think about product testing.

In our webinar, Testing Lab Essentials: Today and Tomorrow Webinar, our team of force measurement experts highlights five critical lessons that go beyond the obvious in product testing. Here is a synopsis of what they shared during the “Do’s and Don’ts” and “FAQs” portion of the technical seminar. The recorded sections of the webinar are at the end of this post, and a summary of the learnings is found here: Testing Lab Essentials Webinar Recap.

Five Truths About a Precision Mindset in Product Testing

#1 – The Best Test Plans Embrace Catastrophic Failure

A core principle in professional test design is planning for the moment the Device Under Test (DUT) actually breaks. This isn’t pessimism; it’s about safety and protecting mission-critical equipment. When a component under immense tension suddenly snaps, the energy released can be violent and unpredictable.

The consequences can include a powerful “ring back” through the load string, like the aggressive snap of an overloaded chain, that damages the sensor, a sudden reversal of load, or an actuator being slammed into the ground. In professional labs, safety and equipment integrity are two sides of the same coin; a setup that is unsafe for people is almost certainly unreliable for data collection. Planning for failure is, first and foremost, a critical protocol to ensure that engineers and technicians are not injured when the unexpected happens.

“When you’re testing something that could break, you have to ask: what happens when that device under test actually fails? Will there be a ring event in the load string? A reversal of load? We must have safety provisions in mind to ensure the most important thing—that people are not injured.”

This is the precision mindset in action: treating failure not as a possibility, but as an inevitability to be engineered and controlled.

#2 – It’s the Peak, Not the Average, That Breaks Things

In dynamic tests involving motors or impacts, it’s easy to focus on the average running force. However, the momentary peak forces are often wildly higher and far more dangerous to your equipment. An electric motor, for example, experiences massive spikes during “startup torques” and “stopping torques” as the system overcomes or resists inertial mass. These peaks can far exceed the average running torque.

The same principle applies to impact loads. A common mistake is to assume that a very short impact is less dangerous to a sensor. In reality, the duration of the event doesn’t matter nearly as much as its peak amplitude. The sensor’s overload rating is based on the maximum force it experiences, even if that force only lasts for a millisecond. Ignoring these peaks is a fast track to damaging expensive measurement devices.

“It’s important to know that the duration of the event is not the problem—it’s the amplitude. It doesn’t matter how long the load cell is subject to a load. It does matter what the peak amplitude is, and it has to be within the safe overload rating of the load cell.”

This illustrates the precision mindset: looking beyond the obvious averages to understand the fleeting, violent moments where failure truly occurs.

#3 – The ‘Environment’ is a Minefield of Leaky Hydraulics and Dropped Wrenches

When specifying equipment, engineers plan for environmental factors like temperature and humidity. But in a busy industrial lab, the “environment” is a minefield of industrial hazards. Leaking hydraulic fluid is a common issue, and some fluids are so aggressive that they can strip the paint clean off a sensor’s protective coating and damage its internal components.

Beyond chemical hazards, there are physical and human-factor challenges. A lab is an active workplace where technicians can accidentally trip over or kick cables, and a dropped wrench can deliver a destructive blow to sensitive equipment. Due to this harsh reality, lab-grade sensors are often specified with rugged features, such as welded stainless steel housings and integrated “connector protectors,” to withstand the daily rigors of an industrial environment.

This is the precision mindset at work: expanding the definition of “environment” to include the messy, unpredictable reality of the factory floor.

#4 – The Most Corrupting Source of Error is Invisible

In a perfect test, all forces would be applied perfectly along a single axis. This is pure tension or pure compression. In reality, this is almost impossible. Off-axis loading is any extraneous force, like a moment (twist) or side load. It is always present, and this misalignment is often the single most significant source of error in a force measurement application. Read Off-Axis Loading 101

This invisible error is so prevalent that premium sensors are engineered with features like eccentric load compensation to reject and minimize its effects mechanically. You can do everything possible to align a test frame, but these forces can still creep in. Experts even use multi-axis transducers as diagnostic tools; by installing one in a standard test frame, they can measure the moments and side loads directly, giving them a clear picture of how well the frame itself is aligned.

This is the precision mindset in its purest form: investing in tools and techniques to see and correct the errors that others don’t even know exist.

#5 – Your Calibration Certificate Is a Health Record, Not Just a Passing Grade

Most people see a calibration certificate as a simple pass/fail document. The certificate is proof that the sensor is working correctly. Lab experts treat it as a vital diagnostic tool for monitoring the long-term health of their equipment. Think of it like a doctor comparing this year’s EKG to last year’s. A single EKG shows your heart is working today, but the comparison reveals trends, subtle degradation, or signs of past trauma. Read Calibration Certificates 101

The expert practice is to compare the new calibration certificate through annual calibration of your sensor with the one from the previous year. This historical comparison can reveal subtle degradation that indicates a problem. For example, a significant “deviation in zero balance” or a change in the “full scale output” from one year to the next suggests an overload may have damaged the load cell or is beginning to drift. This transforms routine calibration from a simple check-box exercise into a powerful tool for preventative maintenance.

Applying the precision mindset means treating data not as a snapshot, but as part of a story that reveals the past and predicts the future of your equipment.

True precision in testing isn’t just about having the best equipment. It’s about developing a mindset that actively seeks out and controls these less-obvious variables. From embracing failure to diagnosing invisible errors, the best results come from understanding that every component, connection, and procedure is part of a complex system that demands relentless attention. Read more in Force Measurement Testing Improves Products and Consumer Safety.

WATCH TO LEARN MORE ABOUT THIS IMPORTANT DISCUSSION

Testing Lab Essentials Webinar - Part 9 Do and Don’t

Testing Lab Essentials Webinar - Part 10 FAQs

ADDITIONAL RESOURCES

Introducing the Interface Consumer Product Testing Case Study

Interface Measurement Solutions for Industry Testing Labs

Interface Case Study Highlights Testing Labs Requirements for Certainty

Testing Labs Choose Interface High Accuracy Products

Interface and Testing Lab Applications

Force Measurement Testing Improves Products and Consumer Safety