Print or Download this Application Note

INDUSTRIES: Aerospace

SUMMARY

 

Customer Need / Challenge

    Develop a system to provide a full range of natural motion for a realistic simulation of reduced gravity environments. The system can simulate future missions to the moon, mars, asteroids, or any other celestial destination. The simulated weightlessness can train crew how to handle a wide range of microgravity activities, including walking, running, and jumping. The system can also be used for surface operation studies, suit and vehicle development, robotic development, and mass handling studies.

Interface Solution

    Model 1100 series load cell is installed in-line with a steel support cable to actively measure the vertical load on the system. A control system, (which includes model 9860 High Speed Digital Indicator), monitors the load cell output and continuously offloads a portion of a human or robotic payload weight during all dynamic motions.

Results

    Using the precise feedback from the load cell, the control system is able to command a motor to raise or lower the subject to maintain a constant offload force. During the simulation, the system actively compensates for the movement of the subject to accurately reproduce a microgravity environment.
MATERIALS

 

  • Model 1100 Ultra Precision Load Cell.
  • CLV-101 Heat Treated Steel Clevis.
  • Model 9860 High Speed Digital Indicator.
HOW IT WORKS
    1. The 1100 series load cell is installed in the vertical axis steel cable.
    2. The subject and simulation exercise are loaded into to system.
    3. The load cell naturally reacts to the continually changing loads on the cable.
    4. The control system (which includes model 9860 High Speed Digital Indicator), monitors the output of the load cell.
    5. The motors are commanded to raise or lower the subject as it runs the simulation.
    6. The subject experiences the sensation of microgravity.