Tag Archive for: rotary torque

Engineering Drivetrain Peak Performance Using Torque and Force
Interface provides force and torque sensors to automotive test labs and engineers for performance testing of drivetrains, the critical mechanical pathway that transfers power to the wheels in vehicles of all types. Direct physical measurement of torque, axial thrust, and multi-axis reaction forces provides the foundational data required to evaluate true efficiency, map dynamic transients, and prevent mechanical fatigue across rigorous automotive test cycles. Interface's AxialTQ is designed for high-accuracy drivetrain testing.

Cycle Testing 101
Interface 101 series highlights cycle testing, which uses load cells, torque transducers, and multi-axis sensors to evaluate functional reliability, kinematic wear, seal integrity, switch actuation life, joint loosening, and mechanical degradation across hundreds, thousands, or millions of operating cycles. Cycle testing is an evaluation methodology used to verify product endurance, track mechanical wear, and establish operational life expectancy under repetitive dynamic loading.

Dynamic Versus Static Torque 101
Understanding the difference between dynamic and static torque is vital in selecting the right torque sensor. Dynamic (rotary) torque measurement is required when the sensor must rotate with the shaft, typically when the component operates at high speeds and/or undergoes significant angular acceleration. The sensor measures the applied or transmitted torque through the rotating shaft. Static (reaction) torque measurement occurs when there is no or negligible angular acceleration of the rotating element, or more commonly, when the measurement is taken on the non-rotating reaction element of a system.

Accelerating Advanced Automotive Testing Using Torque Transducers
Interface rotary and reaction torque transducers are selected for Automotive testing applications due to their accuracy, durability, capacity, and capabilities. Advanced torque transducers drive innovation and facilitate the transition from concept to production in the auto industry shift toward increasing motor performance, fuel-efficient designs, Electric Vehicles (EVs), advanced safety systems, and the integration of Autonomous Vehicle (AV) technologies.

Torque Transducers Review Plus Glossary of Torque Terms
Interface torque transducers measure the twisting force or moment applied to an object. Review our torque glossary, engineering tips, and fundamentals about torque measurement, including a review from Interface's popular Torque 101 webinar.

Rotary Torque 101
Torque is the rotational force that causes an object to turn. Interface rotary torque transducers are versatile sensors that integrate electronics directly onto the rotating shaft. Engineers measure torque using torque transducers that convert a torsional mechanical input into an electrical output signal, typically a voltage or current. Rotary torque transducers are ideal for dynamic applications where continuous rotation is required, eliminating the need for complex wiring and reducing potential points of failure. They are commonly used in measuring torque for engines, gearboxes, robotics, aircraft, medical devices, tractors, and windmills. If it turns, it needs to be measured.

The Future of Automotive Performance Requires Precise Torque Measurement
Interface torque transducers have a driving impact on the automotive industry. Torque sensors transform how automotive engineers design, test, and manufacture vehicles, leading to new inventions and improvements in driving dynamics and production. Interface torque transducers are used in testing brakes, powertrains, electric motors, batteries, fuel pumps and other critical performance and safety components.

Actuators and Sensors Combine Forces in Test and Measurement
An actuator is a device that converts energy into mechanical movement or force. An actuator is responsible for moving and controlling a mechanism…

Interface Primer Dives Deep into Torque Measurement
Interface Torque Measurement Primer provides a comprehensive technical guide to navigate types of transducers, measurement calculations, intallation methods, accessories, mechanical considerations and environmental factors. Torque measurement can be simple or complex, and choosing the suitable transducer requires a deep understanding of your application’s needs. Torque Primer Review Part 2