Subzero Force Measurement to Manage the Chill Effect
The magic of holidays and winter wonderlands often masks a world of rigorous engineering, especially in the equipment that keeps us warm and safe in the bitter cold. When we think of subzero environments, we might picture a quiet, snow-covered mountain, but for a force measurement engineer, that scene is a high-stakes laboratory.
The range of cold-temperature applications is vast, stretching from the heavy machinery used in natural resource extraction to the everyday consumer products we rely on for comfort. Whether it’s a massive excavator operating in an Arctic mine or a new line of weather-resistant wearables, these products must be tested to ensure they don’t fail when the temperature drops.
An obvious setting for required environmental cold-temperature testing is in emulating the slopes. Product engineers are responsible for ensuring skis, bindings, boots, poles, and weatherized safety gear are ready for beginner skiers to professionals, which requires rigorous fatigue and material testing. The simple act of clicking into a pair of skis must be rigorously tested. In subzero temperatures, the materials that make up your bindings are a combination of plastics, metals, and lubricants. All these materials begin to change their physical properties in the cold.
To ensure your safety, ski equipment manufacturers must use high-precision force sensors capable of capturing a wide range of force data. Case in point: verifying that a binding will release your boot during a fall, even if the internal grease thickens or the plastic becomes brittle in freezing conditions, is critical testing. This ensures that the mechanical “release” happens exactly when it should, preventing injury during a holiday trek.
Conditions for Temperature Specifications
Multi-axis sensors are excellent test-and-measurement devices for gathering critical performance data on winter sports equipment. The 2816 2-Axis Axial Torsion Load Cell measures both force and torsion in the same load cell. Either channel can be used independently. Most importantly, the temperature specifications for cold-weather testing are detailed below. It’s an ideal candidate for low-temperature operating range requirements.

Interface load cell engineers recommend examining four temperature-related parameters when selecting the right sensor for extreme-temperature testing.
- Temperature Effect on Zero: The change in zero balance that is due to a change in ambient temperature.
- Temperature Effect on Output: The change in output that is due to a change in ambient temperature. Note that output is defined as a net value, as the zero-load signal is always subtracted from the loaded signal.
- Creep: The change in load cell signal that occurs with time while under load, and with all environmental conditions and other variables remaining constant.
- Zero Return: The degree to which the initial zero balance is maintained after application and release of a load, while environmental conditions and other variables remain constant.
You can learn more in our webinar, Ruggedized Test and Measurement Solutions Webinar.
More Cold Temperature Testing Applications
Beyond the slopes, force measurement plays a part in keeping our homes bright and warm. During a winter storm, ice can accumulate on power lines, adding thousands of pounds of unintended weight. This phenomenon, known as ice loading, can cause lines to sag or even snap the supporting towers. Utility companies now integrate specialized load cells directly into the line hardware. These sensors measure tension in real time, serving as an early warning system. When the force on the cable exceeds a safe threshold due to ice buildup, crews can be dispatched to intervene before a blackout leaves families in the dark.
At the heart of all these frosty applications is the challenge of temperature compensation. Interface force measurement sensors rely on a strain gage, a delicate grid of foil that changes its electrical resistance when stretched or compressed. The problem is that metal naturally shrinks when it gets cold. Without a way to account for this, a sensor sitting in the snow would report a “false” force simply because its internal components are shivering, so to speak.
To remedy the “cold” challenges in load cell design, engineers utilize a sophisticated electrical arrangement known as a Wheatstone bridge. In this configuration, multiple strain gages are wired together to allow the sensor to distinguish between a physical pull and a thermal change. By placing gages that experience the same cold temperature but do not bear the physical load, the circuit can mathematically cancel out the effects of the cold. This ensures that the data remains accurate whether the sensor is in a heated factory or a subzero tundra.
What truly sets Interface apart in these freezing environments is the meticulous mastery of this temperature compensation. In fact, it’s spelled out in the very detailed specifications of our sensors. Learn more about these essential specifications.
While the world of force measurement is vast, Interface engineers are specialists in selecting the exact strain gage characteristics that match the thermal expansion coefficient of the load cell’s metal flexure. By expertly bonding these gages to high-grade alloys chosen explicitly for their stability in the cold, Interface minimizes thermal drift. This prevents the sensor’s zero point from wandering as the temperature drops from a cozy lab to a -45°C testing chamber.
Furthermore, the reliability of Interface products in these subzero testing environments is backed by a rigorous calibration and environmental testing philosophy. Every sensor is designed to withstand the harsh reality of thermal cycling, meaning it can transition from extreme cold to room temperature repeatedly without losing its sensitivity or structural integrity. Read more in Understanding Load Cell Temperature Compensation.
Force Measurement Keeps Us Safe and Warm
When a safety engineer is testing the release of a ski binding or the tension of a frozen power line, they aren’t just looking for a data point. They are seeking industry-leading accuracy that remains unshakable, regardless of the weather.
Load cell engineers at Interface are masters of the invisible technical ballet of strain gage placement, ensuring flexures meet critical specifications across the harshest subzero environments. This level of detail in the gage-to-flexure marriage and the craftsmanship of the internal wiring is why Interface is the trusted partner for assessing the efficiency of aircraft de-icing systems or ensuring that the heavy-duty connectors on heated jackets can withstand the force of frozen hands. It is the difference between a sensor that merely survives cold temperatures and one engineered to deliver peak performance throughout it.
Ultimately, Interface precision is the reason helping manufacturers and engineers keep skiers speeding safely down the slopes, aircraft flying at 30,000 feet in cold air, and the lights burning bright during the icy seasonal conditions.
From the Interface Team, we wish everyone a safe and warm winter and holiday season!