Tag Archive for: specifications

Non-Repeatability 101
Interface 101 defines non-repeatability as the maximum difference between sensor output readings when the exact same load is applied repeatedly under identical loading and environmental conditions. Using load cells, understanding non-repeatability, why it governs a test's practical resolution limit, and how to isolate it from external test-rig anomalies is essential to designing dependable test protocols and accurate analysis.

What is A Load Profile in Test and Measurement?
Interface Tech Talk explores load profile, the time-dependent record of the magnitude, direction, duration, and frequency of mechanical forces a test structure or transducer experiences during operation. Learn key load profile questions prior to sensor selection, engineering tips, use cases, and technical considerations when defining your load profile for your test and measurement applications.

Natural Frequency 101
Interface Natural Frequency 101 defines the inherent rate at which a sensor oscillates when allowed to vibrate freely. Learn how natural frequency and deflection affect dynamic force measurement, how to avoid resonance, and engineering tips for optimizing load cell accuracy. Natural frequency serves as the definitive boundary for the bandwidth of a force measurement system and for structural integrity. Accurate data acquisition from load cells relies on maintaining a clear separation between the application's operational frequency and the resonant frequency of the physical test loop.

Temperature Compensation 101
Interface's 101 Series details load cell temperature compensation, why temperature compensation matters, and key specifications. Prioritizing temperature compensation minimizes measurement uncertainty, leverages the repeatability of thermal shifts, and ensures that test results reflect true mechanical loading rather than environmental interference.

How Do Thermal Specifications Influence Sensor Selection?
Interface Tech Talk details the differences between compensated and operating temperature ranges in load cell specifications. Thermal variables influence sensor accuracy, the mechanics of static deflection. Thermal gradient, material, strain gages, and repeatability are important when selecting a sensor. Only using capacity ignores the realities of the test environment. A load cell's compensated temperature range is the zone where accuracy is maintained by design. The operating temperature range is the boundary for hardware survival.

The Divergence in Force Measurement of Strain Versus Stress
Interface details stress testing versus strain testing using force measurement sensors to quantify material deformation and internal resistive forces. Distinguishing between stress and strain is critical for defining test parameters, selecting sensor capacities, and interpreting data from a material’s elastic and plastic regions.

Interface Data Sheet 101
Interface Data Sheet 101 reviews what to expect from our technical product data sheets. Consider data sheets as a technical roadmap of mechanical and electrical performance information. Interface data sheets include features, a reference image, performance specs, and drawings. The characteristics defined on a product data sheet are used to distinguish successful validation from a system failure by highlighting the individual model's specifications, dimensions, diagrams, characteristics, connectors, and wiring, when applicable.

Bridge Completion Considerations
Interface's use of the Wheatstone bridge is considered world-class in load cell design and for its ability to produce accurate measurements. Selecting the right instrumentation and ensuring proper bridge completion are technical necessities for maintaining the integrity of your force measurement data. Our bridge completion solutions simplify selecting the right instrumentation device to pair with your sensor, making it easier than ever to achieve high-quality measurements.

Elasticity 101
Interface's Elasticity 101 details the importance of Hooke's Law of Physics. In a load cell, we want a material with a very predictable stiffness. If the material permanently deforms or creeps, the deformation value won't return to zero, and your measurements will be inaccurate. A load cell is essentially a mechanical transducer that converts mechanical force into elastic potential energy, which we then capture as data. Understanding how your sensor bends is the first step toward mastering precision force measurement. Learn more in Interface's ForceEDU 101 Series.