How Load Cells Can Go Bad
Load cells are electronic devices that measure the force applied to them. Interface products are made to last, in fact we have many load cells that are in-market and being used for high-accuracy testing that were manufactured decades ago. Why do they last? Quality of design, material construction, build process, calibration, and regular maintenance prolong the life of a load cell.
Like any electronic device, load cells can go bad for a few reasons. It is also important to know that load cells can be repaired. Outside of complete destructive testing, the following issues are most common for how load cell can go bad.
Overloading: Load cells have a maximum capacity, and if they are subjected to a force beyond that limit, they can get damaged. Overloading can cause the load cell to deform or break, resulting in inaccurate readings or complete failure. Preventative options are to use overload protected load cells.
Mechanical and physical damage: Load cells are sensitive devices and can be damaged by impact, vibration, or shock. Mechanical damage can cause the load cell to deform or lose its calibration, resulting in inaccurate readings. Physical damage to devices is often because the load cells are dropped or mishandled during use.
Moisture: Load cells are often used in damp or wet environments, and prolonged exposure to moisture can cause corrosion or damage to the internal circuitry. Environmental exposure to moisture can also cause electrical shorts or create a conductive path between the components, resulting in inaccurate readings or complete failure. Review submersible options if testing in these environments is common.
Temperature: Load cells can be sensitive to temperature changes, and extreme temperatures can cause damage to the internal components. Thermal expansion or contraction can cause mechanical stress, resulting in deformation or damage to the load cell. Interface offers high-temperature and low-temperature load cells options.
Electrical noise: Load cells are susceptible to electrical noise, which can cause interference in the signals and result in inaccurate readings. Electrical noise can be caused by electromagnetic interference (EMI), radio-frequency interference (RFI), or other sources of electrical interference.
Aging: Not all load cells are made the same way. Interface load cells are designed to outlast any testing use for long-periods, we are talking millions of cycles. However, some load cells can wear out over time due to repeated use, exposure to the environment, or other factors. Aging can cause a decrease in sensitivity, accuracy, or stability, resulting in inaccurate readings or complete failure. All load cells need good health checks to stay working at optimal performance.
To avoid load cell failures, it is important to use them within their rated capacity, protect them from mechanical damage, and provide adequate protection from moisture, temperature, and electrical noise. Regular maintenance and calibration services, preferably every year, can also help ensure accurate and reliable performance over time.
What is the best way to determine if a load cell is bad or not working?
There are several ways to determine if a load cell is bad or not working. Here is a reminder of five quick checks:
#1 Visual Inspection: Start by visually inspecting the load cell for any signs of physical damage, such as cracks, deformations, or loose connections. Check for any corrosion or signs of moisture, as well as any visible wear and tear.
#2 Zero Balance Testing: A zero balance test is a quick and straightforward way to check if a load cell is functioning properly. With no weight applied, the load cell should read zero. If it does not, there may be an issue with the load cell or its connections.
#3 Load Testing: Load testing involves applying a known weight to the load cell and checking the reading. If the load cell is accurate, the reading should match the known weight. If there is a significant discrepancy, the load cell may be faulty.
#4 Bridge Resistance Tests: Load cells are typically constructed with a Wheatstone bridge circuit, which can be assessed for proper resistance values. If there is a significant deviation from the expected resistance values, there may be an issue with the load cell or its connections.
#5 Temperature Tests: Load cells can be sensitive to temperature changes, and extreme temperatures can cause damage to the internal components. Evaluating the load cell at different temperatures can help to identify any issues with temperature sensitivity.
Interface provides complete evaluations of any product we manufacture, to determine if the load cell is working properly. To request services, go here.
How does calibration help load cells from going bad?
Calibration is the process of adjusting a load cell to ensure its accuracy and reliability in measuring weight or force. Regular calibration is essential for maintaining the accuracy and reliability of load cells. Interface recommends annual calibration services as a preventative measure and for good maintenance of your force measurement devices.
Calibration helps to ensure that a load cell provides accurate and consistent readings. Over time, load cells can drift from their initial calibration due to environmental factors, wear and tear, and other factors. Regular calibration ensures that any deviations from the standard are detected and corrected, preventing inaccurate readings that can lead to errors in weighing and other measurements.
Load cells that are not calibrated regularly may experience premature wear and tear due to repeated use, leading to damage or failure. Calibration helps to identify any issues early on and prevent further damage, extending the lifespan of the load cell and saving on replacement costs.
Many industries and applications have strict standards and regulations for measuring weight and force. Regular calibration helps to ensure that load cells meet these standards and regulations.
Regular calibration can help load cells from going bad in multiple ways. It can help to prevent inaccurate readings, extend the lifespan of load cells, improve efficiency, and ensure compliance with standards and regulations. Accurate measurements are critical, and calibration helps to ensure that load cells is working properly. Request a repair or calibration service online.
Request a Quote from Interface, The World Leader in Force Measurement Solutions
ADDITIONAL SERVICES
Load Cell 101 and What You Need to Know