Facebook Twitter LinkedIn YouTube
toll-free: (800) 947-5598

Resources Technical Library

Terminology – Abbreviations & Glossary

A helpful diagram for understanding how terms are related.

This document defines the terminology and performance parameters pertaining to engineering specifications of load cell products.

The objective of this terminology standard is to promote effective communication of specifications and to constitute a reference for uniformity.

The definitions herein are generally compatible with common understanding in the load cell community and are an expansion of those found in Load Cell Terminology and Test Procedure Recommendations, Third Edition, 1985, Scale Manufacturers Association, and in OIML International Recommendation R60, 1991 Edition.

This document includes modifications to the definitions in the above referenced standards to correct some of their inconsistencies and inadequacies.

 

 

Load Cell Abbreviations

All abbreviations are case-specific, are not to be pluralized, and do not use trailing periods.

ampere
combined error
degree Celsius
degree Fahrenheit
degree Kelvin
foot
foot-pound 1
full scale
gram
gram force
hertz
inch
inch-pound 2
kilogram
kilogram force
kiloohm
kilonewton
kilonewton-meter
kilopound-foot
kilopound-inch
kilopound (kip)
kilopound force
megaohm
A
CE
°C
°F
°K
ft
ft-lb
FS
g
gf
Hz
in
in-lb
kg
kgf
Kohm
kN
kNm
Klbf-ft
Klbf-in
K
Klbf
Mohm
  meganewton
meter
milliampere
millimeter
millivolt
millivolt/volt
minimum dead load
newton
newton-meter
ohm
ounce-inch
pound
pound-foot
pound-inch
pound force
pound per square inch
rated output
static error band
ton, metric
volt
volt direct current
volt alternating current
watt
MN
m
mA
mm
mV
mV/V
MDL
N
Nm
ohm
oz-in
lb
lb-ft
lb-in
lbf
psi
RO
SEB
t
V
VDC
VAC
W
Note 1 - pound-foot is preferred
Note 2 - pound-inch is preferred


Load Cell Glossary

For convenience, terms which are defined in this standard are printed in UPPER CASE when used in the definition of another term.

AMBIENT TEMPERATURE – The temperature of the medium surrounding the LOAD CELL.

AXIAL LOAD – A load applied along the PRIMARY AXIS.

BAROMETRIC SENSITIVITY – The change in ZERO BALANCE due to a change in ambient barometric pressure. Normally expressed in units of %RO/atm.

CALIBRATION – The comparison of LOAD CELL OUTPUT against standard test loads.

CAPACITY – The maximum AXIAL LOAD a LOAD CELL is designed to measure within its specifications.

COMBINED ERROR – The maximum deviation of the CALIBRATION curve from the straight line drawn between MINIMUM LOAD OUTPUT and MAXIMUM LOAD OUTPUT, normally expressed in units of %FS. Both ascending and descending curves are considered.

CREEP – The change in LOAD CELL SIGNAL occurring with time while under load and with all environmental conditions and other variables remaining constant. Normally expressed in units of % of applied load over a specified time interval. It is common for characterization to be measured with a constant load at or near CAPACITY.

CREEP RECOVERY – The change in LOAD CELL SIGNAL occurring with time immediately after removal of a load which had been applied for a specified time interval, environmental conditions and other variables remaining constant during the loaded and unloaded intervals. Normally expressed in units of % of applied load over a specified time interval. Normally the applied interval and the recovery interval are equal. It is common for characterization to be measured with a constant load at or near CAPACITY.

CREEP RETURN – The difference between LOAD CELL SIGNAL immediately after removal of a load which had been applied for a specified time interval, environmental conditions and other variables remaining constant during the loaded interval, and the SIGNAL before application of the load. Normally expressed in units of % of applied load over a specified time interval. It is common for characterization to be measured with a constant load at or near CAPACITY.

DEFLECTION – The displacement of the point of AXIAL LOAD application in the PRIMARY AXIS between the MDL and MDL+CAPACITY load conditions.

ECCENTRIC LOAD – Any load applied parallel to but not concentric with the PRIMARY AXIS.

FULL SCALE or FS – The OUTPUT corresponding to MAXIMUM LOAD in any specific test or application.

HYSTERESIS – The algebraic difference between OUTPUT at a given load descending from MAXIMUM LOAD and OUTPUT at the same load ascending from MINIMUM LOAD. Normally expressed in units of %FS. It is common for characterization to be measured at 40-60% FS.þ

INPUT RESISTANCE – The resistance of the LOAD CELL circuit measured at the excitation terminals with no load applied and with the output terminals open-circuited.

INSULATION RESISTANCE – The DC resistance measured between the bridge circuit and the case. Normally measured at 50 VDC.

LOAD CELL – A device which produces an OUTPUT proportional to an applied force load.

MAXIMUM AXIAL LOAD, SAFE – The maximum AXIAL LOAD which can be applied without producing a permanent shift in performance characteristics beyond those specified. Normally expressed in units of % CAPACITY.

MAXIMUM LOAD – The highest load in a specific test or application, which may be any load up to and including CAPACITY +MINIMUM LOAD, but may not exceed CAPACITY significantly.

MAXIMUM AXIAL LOAD, ULTIMATE – The maximum AXIAL LOAD which can be applied without producing a structural failure. Normally expressed in units of % CAPACITY.

MAXIMUM LOAD AXIS MOMENT, SAFE – The maximum moment with respect to the PRIMARY AXIS which can be applied without producing a permanent shift in performance characteristics beyond those specified.

MAXIMUM MOUNTING TORQUE, SAFE – The maximum torque which can be applied concentric with the primary axis without producing a permanent shift in performance characteristics beyond those specified.

MAXIMUM SIDE LOAD, SAFE – The maximum SIDE LOAD which can be applied without producing a permanent shift in performance characteristics beyond those specified.

MEASURING RANGE – The difference between MAXIMUM LOAD and MINIMUM LOAD in a specific test or application. It may not exceed CAPACITY.

MINIMUM DEAD LOAD or MDL – The smallest load for which specified performance will be met. It is normally equal to or near NO LOAD in single mode applications and is of necessity equal to NO LOAD in double mode applications.

MINIMUM LOAD – The lowest load in a specific test or application, differing from NO LOAD by the weight of fixtures and load receptors which are attached plus any intentional pre-load which is applied.

MODE – The direction of load. Tension and Compression are each one mode.

NATURAL FREQUENCY – The frequency of free oscillations under conditions of NO LOAD.

NO LOAD – The condition of the LOAD CELL when in its normal physical orientation, with no force input applied, and with no fixtures or load receptors attached.

NONLINEARITY – The algebraic difference between OUTPUT at a specific load and the corresponding point on the straight line drawn between MINIMUM LOAD and MAXIMUM LOAD. Normally expressed in units of %FS. It is common for characterization to be measured at 40-60 %FS.

NONREPEATABILITY – The maximum difference between OUTPUT readings for repeated loadings under identical loading and environmental conditions. Normally expressed in units of %RO.

OUTPUT – The algebraic difference between the SIGNAL at applied load and the SIGNAL at MINIMUM LOAD.

OUTPUT RESISTANCE – The resistance of the LOAD CELL circuit measured at the SIGNAL terminals with no load applied and with the excitation terminals open-circuited.

PRIMARY AXIS – The axis along which the LOAD CELL is designed to be loaded.

RATED OUTPUT or RO – The OUTPUT corresponding to CAPACITY, equal to the algebraic difference between the SIGNAL at (MINIMUM LOAD + CAPACITY) and the SIGNAL at MINIMUM LOAD.

RESOLUTION – The smallest change in load which produces a detectable change in the SIGNAL.

SHUNT CALIBRATION – Electrical simulation of OUTPUT by connection of shunt resistors of known values at appropriate points in the circuitry.

SIDE LOAD – Any load at the point of AXIAL LOAD application acting at 90° to the PRIMARY AXIS.

SIGNAL – The absolute level of the measurable quantity into which a force input is converted.

SPAN – Another name for RATED OUTPUT.

STATIC ERROR BAND or SEB – The band of maximum deviations of the ascending and descending calibration points from a best fit line through zero OUTPUT. It includes the effects of NONLINEARITY, HYSTERESIS, and non-return to MINIMUM LOAD. Normally expressed in units of %FS.

SEB OUTPUT – A computed value for OUTPUT at CAPACITY derived from a line best fit to the actual ascending and descending calibration points and through zero OUTPUT.

SYMMETRY ERROR – The algebraic difference between the RATED OUTPUT in tension and the average of the absolute values of RATED OUTPUT in tension and RATED OUTPUT in compression. Normally expressed in units of %RO.

TEMPERATURE EFFECT ON OUTPUT – The change in OUTPUT due to a change in AMBIENT TEMPERATURE. Normally expressed as the slope of a chord spanning the COMPENSATED TEMPERATURE RANGE and in units of %/°F or %/100°F.

TEMPERATURE EFFECT ON ZERO – The change in ZERO BALANCE due to a change in AMBIENT TEMPERATURE. Normally expressed as the slope of a chord spanning the COMPENSATED TEMPERATURE RANGE and in units of %RO/°F or %RO/100°F.

TEMPERATURE RANGE, COMPENSATED – The range of temperature over which the LOAD CELL is compensated to maintain OUTPUT and ZERO BALANCE within specified limits.

TEMPERATURE RANGE, OPERATING – The extremes of AMBIENT TEMPERATURE within which the LOAD CELL will operate without permanent adverse change to any of its performance characteristics.

TOGGLE – Another name for ZERO FLOAT.

ZERO BALANCE – The SIGNAL of the LOAD CELL in the NO LOAD condition.

ZERO DEAD BAND – Another name for ZERO FLOAT.

ZERO FLOAT – The shift in ZERO BALANCE resulting from a complete cycle of equal tension and compression loads. Normally expressed in units of %FS and usually characterized at FS = CAPACITY.

ZERO STABILITY – The degree to which ZERO BALANCE is maintained over a specified period of time with all environmental conditions, loading history, and other variables remaining constant.

Next: Load Cell Troubleshooting Guide