Facebook Twitter LinkedIn YouTube
toll-free: (800) 947-5598

Industries Automotive and Vehicle Solutions

Brake and Pedal Force Testing

Pedal Force Testing Application
Brake Pedal App Note

To meet certain vehicle safety protocols, pedal force must be measured and recorded. In order to quantify the quality of the braking system, the relationship between pedal force and braking force at the axle must be ascertained, either during an on-road stopping test or in a simulated indoor environment with a dynamometer, where brake force can be measured.

Learn how this is accomplished using an Interface Model BPL Brake Pedal Load Cell along with the Model WTS.

Download the Application Note below.