Mobile Force System
Interface’s solution is to create a portable case with multiple WTS 1200 Standard Precision LowProfile™ Wireless Load Cells, 9812-WTS Wireless Panel Mount Display for Single Transmitters, and the WTS-BS-3E Wireless Base Station. This can connect to the tablet computer to view results. Multiple WTS-ANTE Telemetry Antennas can also extend wireless range. An inverter and rechargeable battery is also installed at the bottom of the foam case so the customer can charge on the go, using a wall outlet or vehicle power outlet.