Technical Advantages and Best Practices for Shunt Calibration

Shunt calibration is essential for verifying and adjusting load cell accuracy by simulating a known load by introducing a shunt calibration resistor. This process utilizes Ohm’s Law to analyze the voltage drop across the resistor, allowing accurate system evaluation without needing physical weights.

Incorporating shunt calibration into your testing and measurement program has key advantages, including rapid system verification, reduced downtime, minimal equipment requirements, repeatable results, and flexibility in integration within measurement systems.

Five Technical Reasons Shunt Calibration Matters in Load Cell Systems

#1 – Verification of Sensor and Signal Chain Integrity

Shunt calibration provides a fast electrical method to ensure the continuity and functionality of the entire measurement chain, from the load cell’s strain gage bridge to the signal conditioning electronics. This is essential as it identifies potential issues such as cable faults, connector problems, or amplifier drift, which can lead to inaccurate readings without physically loading the sensor.

#2 – Precise Scaling and Linearization

Simulating a known load via the shunt resistor accurately scales the load cell’s output voltage to engineering units (e.g., pounds, kilograms, Newtons). More importantly, it helps verify the linearity of the load cell’s response across its operational range. This ensures that the instrument maintains accuracy at various load levels, not just at a single point. Interface offers accessories for load cell systems, including our RCAL Resistors. Use the Accessories Selection Guide to review all options.

#3 – Cost-Effective and Time-Efficient System Validation

While full physical calibration with traceable weights remains crucial for absolute accuracy, shunt calibration presents a significantly faster and more economical method for routine checks and validations. This is especially valuable in large-capacity load cell applications. It enables frequent system checks, reducing downtime and lowering operational costs. Reference a quick validation using our IF500 Load Cell Simulator.

#4 – Mitigation of Environmental and Temporal Drift

Shunt calibration can help detect changes in the load cell’s output due to environmental factors, such as temperature fluctuations or long-term drift in system components. This enables adjustments to compensate for these influences, ensuring measurement accuracy over extended periods and under varying operating conditions.

#5 – Enhanced Diagnostic Capability for System Troubleshooting

Shunt calibration offers a repeatable and predictable electrical signal that can serve as a diagnostic tool. Technicians can quickly isolate and identify issues within the load cell system by comparing the expected output to the actual measured output. This capability significantly decreases troubleshooting time and facilitates faster repairs, ensuring minimal disruption to critical measurement processes.

If you are concerned about the output, it is important always to reference the specifications of any load cell and review the load cell check-up resources. Interface offers complete calibration and repair services if you need a full calibration or repair assessment.

Engineering Tips and Shunt Calibration Process Best Practices

Know Your Resistor: Always use a precision shunt calibration resistor with a known and accurate resistance value.

Follow Manufacturer’s Instructions: Adhere to the manufacturer’s guidelines for the specific load cell and instrumentation. Interface provides detailed specifications, drawings, technical user manuals, and online resources for assistance.

Document Everything: Record the shunt calibration values and any adjustments for future reference. Traceability in test and measurement operations is fundamental.

Verify Connections: Ensure the shunt calibration resistor is connected to the circuit.

Consistent Environment: Conduct the calibration in a stable environment to minimize external factors’ impact.

Regular Checks: Perform shunt calibration routinely to maintain accuracy. Interface recommends a full calibration service annually.

Utilize a Quality Meter: Verify the shunt resistor value with a quality multimeter before and after calibration.

Interface provides a very detailed engineering review of shunt calibration by LaVar Clegg. This whitepaper is available online here.

Shunt calibration ensures that the sensor and its signal conditioning circuitry operate correctly. It also significantly scales instruments, enabling accurate conversions of voltage readings into meaningful weight or force measurements. This is critical as it provides a cost-effective means of verifying sensor health and scaling instruments without physical weights, ultimately contributing to improved accuracy and reliability of measurement data.

Integrating these shunt calibration techniques and best practices and understanding their benefits, such as minimal equipment requirements and flexible integration, is crucial for maintaining the integrity of load cell measurement systems.

Shunt Calibration Review

Interface | Calibration 101

ADDITIONAL RESOURCES

Shunt Calibration for Dummies Reference Guide

Shunt Calibration 101

Shunt Calibration Resistors 101

System Level Calibration

Essential Interface Accessories for Force and Torque Measurement

Interface Calibration Equipment Selection Guide

Calibration-Grade Solutions For Demanding Applications