Interface Sensors Advance Picking and Sorting Efficiency
In logistics and manufacturing, pick and sort refer to the processes of selecting and gathering items to fulfill orders, then organizing them for subsequent steps such as packaging or shipping.
Picking involves retrieving products from a warehouse or storage area based on a customer’s order. This can be done manually or with automated systems.
Sorting entails arranging picked items according to specific criteria such as destination, carrier, or order. The goal is to streamline the final stages of order fulfillment and minimize errors.
These processes are vital in effective supply chain management and are essential to the efficiency of warehouses and inventory operations. When executed accurately, they increase throughput, lower labor costs, and enhance customer satisfaction.
Sensor-Enabled Industrial Automation and Robotics in Picking and Sorting
Modernization of industrial automation and robotics is transforming pick-and-sort applications, surpassing traditional manual methods to achieve faster, more precise, and scalable operations. Robotic systems incorporate load cells and torque transducers into robotic arms equipped with specialized grippers and autonomous mobile robots (AMRs) to enhance workflows. Robots can handle repetitive, strenuous, or hazardous tasks around the clock without experiencing fatigue, thereby boosting productivity and improving worker safety. The accurate measurement of these actions depends on the use of Interface’s reliable sensors.
By integrating with warehouse management systems (WMS) and utilizing advanced sensor data, these automated systems can optimize picking routes, sort items with pinpoint accuracy, and manage inventory in real-time. This not only significantly increases throughput but also allows human workers to focus on more complex, value-added tasks that require critical thinking and problem-solving.
Interface Sensor Solutions for Pick and Sort Applications
Interface’s product line offers robust sensor solutions that enhance the speed, accuracy, and reliability of pick-and-sort systems.
Load Cell Pick and Sort Use Cases
In picking and sorting applications, load cells are used to measure force and load for accurate weighing, quality control, and inventory management..
- Weight-Based Sorting: Miniature load cells, such as Interface’s WMC series, can be integrated into conveyor belts or robotic grippers to weigh items as they are sorted. This helps verify that the correct number of items has been picked or detect missing components in a kit.
- Stock Level Monitoring: Load cells can be installed under shelves or bins to provide real-time inventory counts. As items are picked, the weight change is measured, instantly updating the stock level in the warehouse management system (WMS). This eliminates the need for manual stock checks and reduces the likelihood of errors. Inventory Weighing illustrates this use case.
- Robotic Gripping: LBMU load button load cell is integrated into robotic end-effectors to give a “sense of touch” for a robot. This enables the robot to apply the correct amount of force when picking up fragile or delicate items, thereby preventing damage.
Torque Transducer Pick and Sort Use Cases
Torque transducers measure twisting force and are vital for controlling automated machinery. This is especially important in pick-and-sort equipment.
- Robotic Assembly: In applications where pick-and-sort operations combine with light assembly (such as screwing a cap onto a bottle), torque transducers on the robotic arm ensure the correct amount of torque is applied. This is crucial for maintaining quality and consistency.
- Conveyor System Diagnostics: In conveyor systems, torque transducers monitor the motor’s performance and detect issues like friction, misalignment, or impending motor failure. By measuring the torque needed to move a specific weight, the system can identify problems before a breakdown occurs.
EXTRA: Here is an excellent example of how Interface’s Pillow Block Load Cells can also be used for conveyor belts.
Multi-Axis Sensor Pick and Sort Use Cases
Multi-axis sensors measure force and torque in multiple directions (e.g., X, Y, Z). They are beneficial for advanced robotic applications and when more data improves the efficiency of automation processes.
- Robotic Navigation and Control: Multi-axis sensors enable a robot to gain a detailed understanding of the forces and moments acting on its end-effector. This enables the robot to perform complex tasks with greater precision, such as carefully placing an item on a shelf without colliding with other objects or sorting irregularly shaped items with accuracy. The sensors’ data can be used to adjust the robot’s movements in real-time, enhancing efficiency and adaptability.
- Collision Detection: By continuously monitoring forces, multi-axis sensors can identify unexpected contact with objects or people. This is a vital safety feature in collaborative robotics, where robots operate alongside human workers. Learn more about this cobot application.
TIP: Read more about X-Y-Z Robots and Multi-Axis Sensors are Advancing Automation
By integrating these precision sensors, Interface products enable the next generation of automated pick-and-sort systems to be faster, more accurate, and more reliable, driving significant improvements in supply chain efficiency and profitability.