Tag Archive for: wireless telemetry

Engineering Performance and Safety in Sports Equipment
Interface force measurement sensors allow engineers to push the limits of physics in sporting equipment design and testing. Sports technology use Interface high-accuracy load cells to provide the empirical evidence needed to innovate safely, ensuring that equipment is lighter, faster, and more resilient for professional and casual sports of all types.

Engineering Force Intelligence in Heavy Machinery
Interface load cells and torque transducers provide force intelligence to modernize heavy machinery and enable autonomous control, predictive maintenance, and high-fidelity testing for equipment OEMs. Heavy machinery for construction, mining, and agricultural need force intelligence. Interface’s sensors enable the transformation of standard mechanical joints into smart components that provide the data-driven insights necessary for modern high-production operations.

Interface Solutions for Farming on Land, at Sea, and in the Air
Interface force measurement solutions including load cells, torque transducers, and wireless telemetry systems are important to advancing farming across land, sea, and air. Learn about specific use cases in agriculture, aquaculture, tractor and heavy machinery tests, smart ag drone testing and robotics used in revolutionizing farming.

Dynamic Versus Static Torque 101
Understanding the difference between dynamic and static torque is vital in selecting the right torque sensor. Dynamic (rotary) torque measurement is required when the sensor must rotate with the shaft, typically when the component operates at high speeds and/or undergoes significant angular acceleration. The sensor measures the applied or transmitted torque through the rotating shaft. Static (reaction) torque measurement occurs when there is no or negligible angular acceleration of the rotating element, or more commonly, when the measurement is taken on the non-rotating reaction element of a system.

Civil Engineering Modernization Relies on Force Measurement Data
Interface force measurement sensors and digital instrumentation empower smart infrastructure and civil engineering modernization. From environmental monitoring to construction safety, digital twin testing to material validation, learn why measurement data from load cells is the key to resilience.

Retrofitting Factories with Measurement Solutions
Interface force, torque, and weight measurement solutions for retrofitting factories and modernizing manufacturing can significantly improve operations, efficiency, productivity, safety, and sustainability. Load cells, multi-axis sensors, and load pins can upgrade existing machines and equipment to provide sensor data for predictive maintenance, quality control, and improving durability.
Tag Archive for: wireless telemetry

Search and Rescue Robots
Interface suggests using multiple force sensors to test the search and rescue robot. The robot's wheel torque can be measured using a T14 Slip-Ring Shaft Style Rotary Torque Transducer, installed inside of the robot's wheel alongside the motor. Two ConvexBT Load Button Load Cells are used in the grips of the robotic arm to measure the amount pressure being applied.