Energy

Interface force measurement solutions are used in every facet of energy production from research and exploration, to monitoring equipment especially our Oil Gas Energy Sensors. Load cells and torque transducers assist oil, gas, wind, coal, solar, and emerging energy companies to fuel the world.


oil, gas, wind, coal, and solar applications


Energy Overview

Interface force measurement solutions are used in every facet of energy production from research and exploration, to monitoring equipment especially our oil and gas energy sensors. Load cells and torque transducers assist oil, gas, wind, coal, solar, and emerging energy companies to fuel the world. When our petroleum customers came to us requesting load cells that could withstand up to 30,000 psi and 500°F, we met the challenge with custom application-specific solutions.

Harsh Environments

Our moment and temperature compensated LowProfile™ load cells use proprietary alloy strain gages to provide the most accurate readings possible in the harshest environments, such as downhole drilling, wirelines, pipelines, and wind turbines.  Interface tests every LowProfile™ load sensor for accuracy and temperature specifications, and moment compensates each unit to minimize sensitivity to extraneous loads. Using eight proprietary strain gages per sensor, our 4mV/V output which exceeds most other load cell performance specifications.

Windmill Energy

Our torque transducers have been used in instances for windmill energy. A customer wanted to improve their windmill by monitoring the torque being created by the windmills power ramps. Installing our T2 Ultra Precision Shaft Style Rotary Torque Transducer between the windmill propeller and the electric generator of the windmill, it resulted in accurate testing. Shaft Style Torque Transducer Couplings were also installed to ensure stability. This resulted in our customer being able to determine the optimal blade pitch for their windmill, thus being able to generate more energy.

With a variety of load cells, load buttons, force transducers, torque transducers and other Oil Gas Energy Sensors available, our applications engineers can help you design a measurement solution for your energy production needs.

Interface Pressure Compensated Downhole Load Cell

The downhole environment poses many challenges for well-drillers, operators, tool-string designers, and other engineers in the oil and gas industry. Obtaining accurate force measurements poses some real challenges in certain use cases based on the sensor technologies used and while these types of solutions are available, they fall short in performance, reliability, or capability. For example, the oil and gas industry has used “wet” load cells to monitor forces on their downhole load strings. These downhole load strings are equipped with a variety of sensors, and they travel down thousands of feet during exploratory drilling operations. The problem with wet load cells is that they don’t hold up for extended use in wells that extend several thousand feet underground and where there are extreme pressures and temperatures in a caustic environment. To address this issue, Interface created a “dry” load cell that protects the sensitive parts with innovative design, reduces the number of sensors required in the customer’s downhole load string, and allows the load cell to last 10 years or more.

Energy Solutions from the IQ Blog

Interface Helps Power the World

As technology and infrastructure have advanced to accommodate various forms of energy collection, the role of force measurement in the test and manufacturing of these machines has grown significantly. As a precision force measurement solutions provider, Interface has been a […]

Announcing the Launch of the Interface Pressure Compensated Downhole Load Cell

Interface is excited to announce the release of a new downhole solution for the energy industry, the Interface Pressure Compensated Downhole Load Cell (IPCD). The IPCD is a Wheatstone bridge foil-gaged-based force measurement solution using proprietary compensation methods and designed […]

Fueling Global Demand for Interface Solutions

Increasing demand for quality, accurate and reliable sensor technologies is global.  Interface products are used on every continent and across all types of industries. As manufacturers and product innovators make advances in what they build and test, there is a […]

Infrastructure Industry Relies on Interface Force Measurement

The safety and stability of the structures and facilities that are used by towns, cities, organizations, governments and countries are essential to their successful operations. In the design and construction, it is a requirement to ensure that every component measures […]

Why Machine and Equipment Manufacturers Choose Interface

For innovators in the equipment and components manufacturing industry, data is everything. Quality data can make the difference between average and high-quality products and every bit of information gathered allows OEMs to make improvements that go a long way in […]

Interface Solutions Designed for Infrastructure Challenges

All infrastructure, big and small, needs to be designed with safety and durability in mind. Take for instance the massive amount of design, engineering and quality control that goes into a suspension bridge requires testing before and after it’s built. […]

Interface Explores Maritime Applications Near and Offshore

Land, air, and sea are all the places where Interface force measurement devices are used to test and confirm product designs and measure real-time functions of equipment. Interface has long provided an array of sensor solutions for the maritime industry. The solutions […]

Faces of Interface Featuring Brian Peters

It is not every day that we get to share a story about an accomplished engineer and sales leader who also drives a racecar. Let us introduce you to our Global Sales Vice President, Brian Peters, and our Chief Applications […]

Hazardous Environment Solutions from Interface

There are hundreds of thousands of engineers and manufacturers that spend their days working in hazardous environments. Whether its operating inside of facilities with large machines with intricate moving parts, working hundreds of feet in the air repairing a bridge, […]

Interface’s Sustaining Role in Arizona and the Global Business Ecosystem During COVID-19

For more than half a century, Interface has had the privilege of serving a wide variety of industries and helping our customers test, design, and manufacture products and infrastructure essential to everyday life. Our purpose at Interface defines our commitment […]