Interface and Infrastructure Markets Form a Perfect Partnership
Infrastructure projects are growing, as investment continues to climb for projects related to rebuilding, renewing and innovating applications in this sector. These global investments come from public and private organizations as demands to address roads, bridges, water supplies, transportation, energy systems, and broadband requirements for the 21st century grow.
Experts who focus on infrastructure acknowledge these are means for civil existence and prosperity. Interface understands that our role in supporting the design, testing, manufacturing, constructing and maintenance required in infrastructure needs a top supplier of force measurement solutions.
Interface force measurement solutions have and are currently used around the world for infrastructure projects including bridges, generators, dams, waterways, transportation structures, construction projects, cranes and lifting apparatus, and heavy machinery.
Interface supplies durable and accurate sensor technologies used in testing equipment, technology, vehicles, tools and machines used in all types of infrastructure subsectors. We also find our products often designed into structures for regulatory and safety monitoring, whether that be to maintain tunnels or support wind generating farms.
Interface details force measurement products we commonly provide to those working and supporting the infrastructure sector in our Infrastructure Solutions Brochure. You can see some of these products in our Infrastructure Solutions video.
Interface load cells, load pins, instrumentation, multi-axis sensors, and torque transducers are top choices for those engaged in infrastructure projects and testing. Sensors are commonly used in measuring the related hardware used for industry products and structures. The types of infrastructure projects that Interface has supplied measurement solutions for includes transportation systems, communication structures, water and electrical facilities, and numerous inventions that are used to build, support, and maintain them, as outlined in Infrastructure Projects Rely on Interface.
Our expert engineers can help design customizable force measurement solutions for all types of applications that require sensors for OEMs and to be used in the actual structure for continuous measuring and monitoring. We have engineered sensor products used for civil engineering designs and infrastructures used in structural monitoring, vibrational monitoring, load bearing testing, tunnels, bridges, and road construction. The range of projects are broad, so we are highlighting a few below that highlight our capabilities when accuracy, quality and reliability matter in design, testing, construction, and assessing current and limitations for safety requirements.
Hydraulic Jacking System Testing
An equipment manufacturer needed to test their hydraulic jacking system’s ability to lift heavy loads and objects, like a bridge during construction. They wanted to monitor the forces being applied to ensure the hydraulic jack is not only safe to use, but works well enough to avoid any potential structural issues. Interface’s 1200 Standard High Capacity Load Cell can be attached in between the hydraulic jack and a heavy load. The load cell measures the forces of the hydraulic jack as it lifts the load cell located in between the jack and the object. With the 9890 Strain Gage, Load Cell, & mV/V Indicator, the customer is also able to see the results in real-time. Read more here.
Aerial Lift Overload Control
A manufacturing company for aerial lifts wanted to test its self-propelled boom lift to ensure it can operate at heavy capacities when in use, and at different angles. They also wanted to prevent any accidents in case of a lifting overload, for the safety of any working individual who uses it. Interface’s solution was to attach the 3A160 3-Axis Force Load Cell to the bottom of the bucket of the boom lift. The multi-axis sensor provides high accuracy results, which were displayed using the 920i Programmable Weight Indicator and Controller in real time. The manufacturing company tested their aerial boom lifts and determined it was safely operable when maximum capacities has been reached in use. Read more here.
Truck Weighbridge Monitoring
A transportation company needed to record the weight or loads being carried by their vehicles. They would like a wireless weighing bridge that is able to transmit, log, and display the results in real time. Interface suggests installing multiple WTS 1200 LowProfile™ Load Cells under a weighbridge. When a truck drives over it, the load cells will transmit the force results wirelessly to the WTS-BS-4 Industrial Base Station connected to the customer’s PC with provided Log100 software. The WTS-LD2 Wireless Large LED Display can also display the weight inside for the driver to see in real time. The customer was able to measure, log, and graph the different loads their trucks carried wirelessly onto the weighbridge with success, providing for safe passage across transportation ways. Read more here.
Hydropower Turbine Generator Monitoring
A customer wanted to monitor and detect any turbine generator faults in their hydroelectric power plant located on a river. Interface’s solution was to use the T2 Ultra Precision Shaft Style Rotary Torque Transducer and attach it to the turbine generator with Interface’s Shaft Style Torque Transducer Couplings. When water from the river pushes through the penstock to the outflow, it moves the turbine blades, creating electricity through the generator shaft. Torsion measurements can be graphed and logged with the 9850 Torque Transducer and Load Cell Indicator catching any unusual fluctuations and vibrations. Using this solution, the customer was able to monitor, graph, and log the torque measurement results of the turbine generator. Read more here.
Bridge Seismic Force Monitoring
A customer wanted to monitor seismic activity that occurs to a bridge by using force sensors and then continuously monitoring bridge forces before, during and after earthquakes occur. The customer also preferred a wireless solution so they would not need to run long cables on the bridge. Using Interface’s LP Load Pin custom made to fit their needs along Interface’s WTS Wireless Telemetry System for continuous force monitoring the designed solution was able to take place without long cables. The solution allowed the customer to monitor continuous loads, log information to the cloud and review information. Read more here.
Interface’s work with all facets of the infrastructure industry spans far and wide. Interface is a supplier of choice and key partner for providing reliable sensors and instrumentation solutions used in testing and monitoring of both the infrastructure and the equipment used to upgrade and refine it.
ADDITIONAL RESOURCES
Infrastructure Industry Relies on Interface Force Measurement
Infrastructure Projects Rely on Interface
Interface Solutions Designed for Infrastructure Challenges
Monitoring the Seismic Force of a Suspension Bridge