Innovative Interface Load Pin Applications
A load pin, which often replaces a standard clevis or pivot pin, is a strain gage sensor that measures the force applied across the device. The strain gages are installed within a small bore through the center of the pin. Interface load pins have been used in a wide variety of projects across many industries.
Load pins are a simple, but highly powerful sensor that provides data collection for accurate and frequent measurement. The load pin can replace a bolt, clevis, sheave, and an equalizer pin, as well as other load-bearing components to measure tensile and compression forces.
Machined from high tensile stainless steel, Interface load pins are suitable for exposed situations including seawater. We offer standard sizes of load pins between 1.1K lbf to 3.3M lbf (500kgs to 1500 MT). We also offer wireless load pins. Interface load pins are custom manufactured to meet specific dimensional requirements for each application, as detailed in our Use Cases for Load Pins webinar.
The most commonly referenced applications for load pins are for overhead equipment like cranes and lifts. Through ingenuity of engineers and our customers, load pins are rapidly expanding in popularity for infrastructure, aerospace, maritime, agriculture, and industrial use cases. The load pins of today are used to test and measure force, load, and weight in a much larger variety of applications. They are also growing in demands due to their wireless capabilities for both short and long distances. This includes uses not only for cranes and lifting devices, as well as construction equipment, industrial machines, nautical craft and equipment, aerospace structural environments, and civil engineering applications.
Infrastructure investment and projects around the world are on the rise. Investments in transportation ways like highways, waterways, bridges, mass transit, water supplies and power generation are frequently in demand of load pin solutions for use in all phases of the projects, from construction to maintenance and real-time monitoring. Some of these examples are highlighted in Infrastructure Projects Rely on Interface.
Interface has a great deal of experience supplying ruggedized and standard use load pins for testing. Our load pins are highly demanded in the infrastructure industry not only due to the accuracy and reliability of our sensors, but also due to the fact that we offer a myriad of communication channels to offer both wired and wireless solutions. As requirements are made to repair and rebuild public infrastructure resilience, equity, and safety for all users are key criteria in design and build stages. This is where Interface load pins are key to the solution, for durability, accuracy, quality, and ease-of-use.
Interface captured a few application examples of how our load pins are used for different types of projects, from maritime submersibles to monitoring new bridges during earth’s constant shifting.
AEROPSPACE: Landing Gear Joint Testing
A global manufacturer in aerospace needs to test their new assembly and design by testing its landing gear joints. They want to ensure there are no flaws in the gear shock absorber design and can handle the applied forces when the craft lands from a flight. Interface’s WTSLP Wireless Stainless Steel Load Pins can be installed and replace the normal pin joints. The aircraft undergoes multiple drop tests at different heights, where the forces are applied on the load pins which then transmits the measurement data. The force results are transmitted wirelessly to the WTS-BS-4 USB Industrial Base Station and the WTS-BS-1-HA Handheld Digital Display for multiple transmitters. Read more about this load pin use case here.
MARITIME: Quick Release Hooks (QRH)
A customer wanted to test their quick release hook (QRH) system when their vessels are docked. They wanted to ensure the mooring lines are secured, but also, the quick release hooks were able to be easily and safely released. Interface’s WTSLP Stainless Steel Load Pin was installed into the quick release hook, where forces from the mooring lines can be measured and displayed when paired with the WTS-BS-4 USB Industrial Base Station. The load tension forces were displayed in real-time on the customer’s PC or laptop. The WTS-RM1 Wireless Relay Output Receiver Module alarm could also be triggered for the customer when maximum safety work load capacities have been reached or are overloaded. Using this solution, the customer was able to determine if their quick release hooks worked effectively within the safe working limit specifications, and was aware of any potential overload situations. Read more here.
INFRASTRUCTURE: Bridge Seismic Force Monitoring
A customer wanted to monitor seismic activity that occurs to a bridge by using force sensors and then continuously monitoring bridge forces before, during and after earthquakes occur. The customer preferred a wireless solution so they would not need to run long cables on the bridge. Interface helped to develop its LP Load Pin, which were custom made to fit their needs along Interface Inc. WTS Wireless Telemetry System continuous force monitoring was able to take place without long cables. Using this solution, the customer was able to monitor continuous loads, log information to the cloud and review information. Read about this solution here.
AGRICULTURE: Tractor Linkage Draft Control
A farming operation needs to measure the forces applied on their tractor’s draft control, between the tractor and any linked on attachments. Measuring the force helps the farmer sense any strains on the hitch of the tractor, and will be needed in order to apply any specific settings to the draft control when the tractor encounters rough terrain. Interface’s WTSLP Wireless Stainless Steel Load Pin is a wireless load pin that can be installed directly in the hitch, replacing the normal shear pin of the tractor. Force results are transmitted wirelessly to the WTS-BS-4 USB Industrial Base Station, where they can view the results on a computer using Interface’s WTS toolkit. The customer can also view results on the WTS-BS-1-HS Handheld Display for Single Transmitters in real-time. Read more about this IoT Agriculture solution here.
INDUSTRIAL AUTOMATION: Crane Block Safety Check
A customer wanted a system to detect if their crane block can lift heavy loads securely, in order to keep working conditions and personnel safe. If lifting capacities are exceeded, the customer wanted a system to alarm them in real-time. Interface’s WTSLP Wireless Stainless Steel Load Pin replaced the existing load bearing pin in the crane block in order to measure the force being applied by the heavy load. The data was transmitted and displayed through both the WTS-BS-4 USB Base Station (when paired with the customer’s supplied PC computer/Laptop) and the WTS-BS-1-HA Wireless Handheld for real-time results. The WTS-RM1 Wireless Relay Output Receiver Module could also trigger an alarm when maximum capacity has been reached. The WTSLP Wireless Stainless Steel Load Pin, combined with the WTS products, was able to measure and determine force applied the moment a heavy load is lifted. The results were transmitted wirelessly, and ensured the customer whether or not the crane block was safely operational during production.
Are load pins the right solution for your project? Contact our load pin application engineers to learn more.
ADDITIONAL RESOURCES
Load Pins, Tension Links, and Shackles
Recap of Use Cases for Load Pins Webinar
LP-TL-Shackles-Brochure