Deeper Dive into Maritime Solutions from Interface
The maritime industry is one that Interface products are uniquely designed for based on the extensive technical requirements and challenges needing ruggedized solutions to perform in harsh environments. Like any industry that manufacturers vehicles and large machinery, the maritime industry requires supremely accurate force measurement systems for performance and safety testing and ongoing infield use. However, the maritime industry has the added challenge of needing measurement technologies and equipment that function in offshore and submersible environments, and that can hold up to intensely cold temperatures while still providing accurate data.
In our new maritime case study, we take a deeper dive into some of the use cases and solutions we provide to the industry.
Interface offers an entire line of products commonly used in maritime applications of all types, including our performance load cells, load pins, load shackles, tension links, wireless instrumentation, miniature load cells and engineered-to-order products. Interface products are used to test and measure continuous performance for waterborne vessels, dock equipment such as cranes and lifting apparatus, submersible devices, and offshore machines. Interface maritime solutions are made to survive in the conditions conducive to the industry, allowing users and component manufacturers to test and operate equipment that guarantee accuracy and reliability in performance. Read more about solutions for maritime in this post.
To highlight some of the maritime applications and use cases of our products, the recently published case study exemplifies why Interface maritime solutions are aligned to the industry’s high standards and requirements for force and torque test and measurement, and weighing.
New Maritime Case Study
Interface has been a longtime leader in supplying products to the maritime industry. From hydrofoil testing to yacht rigging inspection, and even on the enormous cranes used on shipping docks, we provide solutions for a wide variety of applications in maritime. The U.S. maritime industry employs over 400,000 workers and according to the National Marine Manufacturers Association (NMMA), annual sales of boats, marine products and services were estimated at $42B. This includes organizations that develop hardware to support shipyards, marine terminals, fishing, aquaculture, seafood processing, commercial diving, and marine transportation.
Interface is the vendor of choice for maritime, for example we offer load cells that can wirelessly transmit data through underwater applications and harsh weather conditions. These load cells can survive through underwater submersions at different capacities, and still be able to relay information to those at the surface level. Interface load cells can also regulate harsh maritime situations such as underwater tension lines, underwater oil drilling, and storm and tsunami monitoring.
Interface wireless load pins, load shackles, and tension links are ideal for sea applications paired with our different wireless sensor transmitters, receivers, and handheld displays. Our Wireless Crosby Bow Load Shackles are used for mooring line tension testing and rigging inspections. Our load shackles are also inter-changeable with our WTSTL Wireless Tension Link Load Cell. The WTS-BS-4 Wireless Industrial USB Base Station is a popular transmitter that gives outstanding coverage and can be easily paired with one of our handheld displays such as the WTS-BS-1-HA Wireless Handheld Display for Multiple Transmitters, or the WTS-BS-1-HS Wireless Handheld for Single Transmitters.
For the full case study, click here.