Calibration for Crane Scale and Dynamometer Applications
Interface is well-known for excelling at calibration services for load cells. Did you know this service excellence extends to dynamometers and crane scales?
Interface can calibrate dynamometers and crane scales with capacities of 100,000 pounds of force or more. This family of devices is often found in industrial, commercial, energy, military, and aerospace industry applications.
Crane scales are used as overhead weighing solutions ranging from light to heavy capacities and are normally placed in the load string of a crane. The devices provide crane overload protection, as well as information about the handling of bulk material. Some models are equipped with wireless communications to allow monitoring from safe distances at multiple locations.
Dynamometers, which are sometimes referred to as tension links or dyna-links, are also used in many overhead weighing applications. These devices are usually smaller and lighter than crane scales allowing them to be used in vertical and horizontal positions. In addition to weighing and crane overload protection applications, dynamometers are often used for crane certification, elevator certification, and several other inline test and measurement applications.
What really makes Interface different when it comes to our calibration services for crane scales and dynamometers?
First, our calibration equipment is custom-made for this exact purpose. That means we don’t take a one-size-fits-all approach to your specific calibration needs, giving you the peace of mind that your calibrations are done correctly.
Second, we have decades of experience providing industry-leading service and putting our customers first. We are sought out for this service for a reason—because we get it done right.
Additionally, Interface does not use hybrid systems for its calibrations. We use direct force application and NIST traceable force standards with customized fixture assemblies for each type of equipment. These important distinctions allow us to focus on providing the best-accredited calibrations for crane scales and dynamometers available in the industry.
Not only are we recognized experts in calibration services, but Interface is also known globally for reliability, accuracy, and longevity of its products. Interface manufactures force products which are used worldwide in test and measurement applications, as well as our own renowned metrology lab. Our specialized engineering and metrology teams pay close attention to the performance data of these standards. With proper maintenance and regular calibrations by Interface, we provide assurance that load cells are operating at the highest standard.
Interface understands that aerospace and military engineering professionals cannot wait long periods of time to receive their load cells after calibration service. We are known for our quick turnaround time. We make sure load cells, crane scales, dynamometers, and other force measurement equipment is calibrated to perfection expeditiously, to prevent significant disruption to any operations.
“Interface’s 51 years of experience in manufacturing and calibrating force measurement devices makes us one of the largest and most sought-after calibration service providers in the world. Our team follows strict standards and protocols to make sure our customers are receiving the best calibrations possible.” Mike Cobb, Director of Services.
This year, Interface introduced a new Tiered Calibration Services Program to offer customized and expedited services. No matter the tier of service, Interface services receive a warranty and all our service is ISO 17025 accredited calibration service. To schedule a service, visit here.