Tag Archive for: electrical

Load Cell Electrical Components, Connectors, and Wiring Standards
Interface provides technical specifications, pinouts, and wiring documentation for load cells, torque transducers, multi-axis sensors, and instrumentation for each product. Achieving high-accuracy measurement data depends completely on the integrity of the electrical connections between the sensor and the instrumentation. Simple wiring errors or incorrect pin mapping can result in inverted data, thermal drift, or irreversible damage to components in the data acquisition system. Interface Support offers Electrical Wiring and Diagrams resources, including cable, connector, and assembly wiring colors and references.

The Divergence in Force Measurement of Strain Versus Stress
Interface details stress testing versus strain testing using force measurement sensors to quantify material deformation and internal resistive forces. Distinguishing between stress and strain is critical for defining test parameters, selecting sensor capacities, and interpreting data from a material’s elastic and plastic regions.

Resistance Output Versus Rated Output
Rated Output (RO) is the dynamic electrical signal that directly represents the applied mechanical force. Resistance Output is a static electrical characteristic of the load cell's internal circuitry. When you are performing force measurements, you are primarily interested in the Rated Output. This value, in conjunction with your excitation voltage, enables you to accurately convert the measured millivolt signal into engineering units of force in lbf or Newtons. Discover how load cells work at the ultimate force measurement resource hub, Interface ForceEDU.

Navigating Load Cell Calibration and Repair Services
Interface details the difference between load cell calibration services and repair services. Discover how to decide between the types of services. Get tips to maximize accuracy and extend your equipment's life, considerations when selecting a service, and how to request a service today.

Load Cell Wiring 101
Load cell performance depends significantly on the electrical system. Wire colors and pin assignments are essential when assembling your load cell using connectors, cables, and instrumentation. Interface provides a complete electrical wiring resource for sensor models, wire colors, pins and specifications. Wiring mishaps are a source of electrical connection errors, leading to inaccurate readings, equipment damage, or even safety hazards.

Interpretation of Force Measurement System Errors
Interface clarifies error source terms. Understanding the potential sources of error is crucial to accurate force measurement. Often, terms like resolution, repeatability, and reproducibility are used interchangeably, leading to confusion. It's important to remember that these are system parameters.

Load Cell Performance Starts by Design Webinar
Interface ForceLeaders event Load Cell Performance Starts by Design provides a detailed engineering perspective of sensor technologies designed for precision force measurement. The technical webinar features an advanced perspective on specifications and criteria to perfect the performance of the world's best test and measurement devices to measure force.

Detailing Sensor Rated Output Millivolts Per Volt
Interface sensor specifications state rated output, expressed in millivolts per volt (mV/V), as the electrical output of a load cell, multi-axis sensor, or reaction torque transducer in mV/V of excitation at the rated load. It essentially expresses a load cell's sensitivity. RO represents the change in output voltage in millivolts of the load cell relative to a change in the excitation voltage in volts applied to it.

Why Is Load Cell Zero Balance Important to Accuracy?
Several factors go into the accuracy and consistent performance of a load cell. These factors include non-linearity, hysteresis, repeatability,…