Addressing Off-Axis Loads and Temperature Sensitive Applications
As technology progresses, one of the main differences we see over years and years of iteration on a wide range of consumer and commercial technology is miniaturization. There are hundreds of thousands of examples of advancing technology that went from the room-size of a mainframe decades ago, to a handheld device today. As technology grows more compact and convenient, the equipment used to design, test and manufacture these devices has to follow suit.
This is one of the driving factors for Interface to increase the product types and capabilities in our Load Button Load Cells and Interface Mini Load Cell products. Interface’s Load Button Load Cells are designed for customers who require the measurement of forces in a very confined space. They provide the most accuracy in as little space as possible. Diameters range from 1 inch to 3 inches, with heights from 0.39 inch to 1.5 inches.
For many years, load button load cells have been sensitive to off-axis, eccentric or misaligned loads. This means that if the load is not exactly perpendicular to the surface it’s resting on, the data could become skewed or inaccurate. All on-axis load generates some level, no matter how small, of off-axis extraneous components. This can cause a variety of challenges including slight inaccuracies and reduction of the load cells overload capacity.
With Interface’s family of load button load cells, we bring premium accuracy and repeatability, even under eccentric angular loading. The shaped load button has a spherical radius to help confine misaligned loads to the primary axis of the cell. Our design engineers and force measurement experts have purposefully tested applications under a wide variety of load conditions to ensure that the our load button series can continue to deliver premium performance. We have been extremely pleased with the results and continue to advance our offerings, including the soon to be released precision focused ConvexBT load button load cells.
The load button load cells’ size has in the past precluded the use of internal temperature compensation. We have redesigned our ultra precision product line of load buttons to ensure that this is no longer something the user has to account for when testing a product in certain environmental conditions.
Interface engineers have eliminated this issue by taking the technology out of the load button load cells cable and designing it back into the product. This ensures that temperature-sensitive applications do not suffer from errors caused by the load cell being exposed to different environmental conditions than the cable.
These new features open new possibilities to test compression force on a broader range of products and environments. To learn more about our ultra precision Load Cell Load Buttons and how it can make a difference in your design and testing process when dealing with tight and confined spaces, contact our Application Engineer experts here.
To see the complete line of Load Button Load Cells, visit here. Watch for the release announcement of our new ultra precision ConvexBT product coming out this month.
Contributors: James Richardson, Interface Mechanical Engineering Manager and Ted Larson, VP Product Management and Marketing
Source: Interface Load Cell Field Guide