Tag Archive for: shear

Understanding Dual Shear Load Cells
Interface dual shear load cells are strain gage sensors supported at both ends, with the force applied directly at the center of the beam. A double-ended shear beam load cell design is used in the high-performing Interface LowProfiles and load pins. The dual-ended design distributes force symmetrically across two matched shear webs. Strain gages are bonded to the machined webs inside the beam and configured in a full Wheatstone bridge circuit to convert mechanical shear stress into an electrical mV/V signal.

Core Measurement Fundamentals of Force, Stress, and Strain
Understanding differences in measuring force, stress, and strain, and how Interface's load cells accurately measure changes in objects, will help you better prepare to maximize the potential of your force measurement solutions for critical applications.

Comparing Shear Versus Compaction Force Measurement
Interface load cells are used in shear and compaction force measurement. Understanding the differences between shear and compaction is determinative, as it directly impacts applications, sensor choices, and output data for testing analysis. Learn about shear force versuse compaction, also known as compressive, measurement, applications and load cell types. This understanding aids in making informed test and measurement decisions in material science, mechanical engineering, and industrial automation.

Force Measurement is Fundamental in Material Testing
Interface load cells, multi-axis sensors, and data acquisition systems are used for material testing. Common uses of force measurement in material tests include applications to measure hardness, torsion, strength, compression, bending, shear, impact, creep, fatigue, and nondestructive capabilities. It is common to have our 1200 LowProfile load cells installed into material testing machines at test labs and onsite. We also supply a variety of miniature load cells and load pins for material testing, depending on the type of equipment and environment used for tests.