Tag Archive for: static

Dynamic Versus Static Torque 101
Understanding the difference between dynamic and static torque is vital in selecting the right torque sensor. Dynamic (rotary) torque measurement is required when the sensor must rotate with the shaft, typically when the component operates at high speeds and/or undergoes significant angular acceleration. The sensor measures the applied or transmitted torque through the rotating shaft. Static (reaction) torque measurement occurs when there is no or negligible angular acceleration of the rotating element, or more commonly, when the measurement is taken on the non-rotating reaction element of a system.

The Crushing Reality of Impact Loads
Interface details the importance of understanding impact loads, which introduce a dynamic element that significantly amplifies the force experienced by the load cell. Physics are important in force measurement, understand how to protect your sensors from overload and damage from impact. Learn about impact drop testing and key considerations when choosing a sensor.

Reaction Torque 101
Interface reaction torque transducers offer exceptional measurement accuracy in static and low-rotation applications. A reaction torque transducer uses strain gage technology. These sensitive components deform slightly when subjected to torque. The static, stationary nature simplifies integration into test setups and existing systems. They are available in various configurations for diverse applications, including shaft, flange, and square drive.