Tag Archive for: moment compensation

Seven Essential Terms in Force and Torque Measurement
Force and torque measurement rely on precise technical vocabulary. Load cell terms like side load, moment, and ultimate overload determine a sensor's accuracy, lifespan, and safety. Understanding seven terms can prevent failure, loss of testing data or protect the investments in measurement systems.

Moment Compensation Relevance for Aerospace, Robotics, and Structural Testing
Moment compensation is a fundamental engineering principle that ensures stability and accuracy by counteracting unwanted forces. Industries like aerospace, robotics, material and structural testing know precision is non-negotiable. At Interface, the moment compensation principle is a core part of our load cell design best practices, making our force measurement solutions a decisive component in some of the world's most demanding applications.

Load Cell Performance Starts by Design Webinar Recap
Interface Load Cell Performance Starts by Design emphasizes the engineering perspective in designing the world's leading force measurement devices used to test everything from rockets to medical devices. In the recap and webinar recording, learn about flexures, strain gages, specifications, engineering design tips, types of load cells and more in this advanced technical load cell seminar.

Load Cell Performance Starts by Design Webinar
Interface ForceLeaders event Load Cell Performance Starts by Design provides a detailed engineering perspective of sensor technologies designed for precision force measurement. The technical webinar features an advanced perspective on specifications and criteria to perfect the performance of the world's best test and measurement devices to measure force.

Low Profile Load Cells versus Simple Single Column Load Cells
The Interface LowProfile Load Cell, a pancake design, is dramatically better than the simple single column cell in every respect. The low profile design outperforms the single column design. The overall proprietary Interface LowProfile design is more compact, with all the components bonded to the flexure structure, making it better able to withstand the 100 million-cycle fatigue life. Our standard 1200 “Blue” LowProfile Load Cell is the most popular load cell in the market and is used in testing labs and industry applications worldwide.

What is Moment Compensation?
Every Interface LowProfile™ load cell is moment compensated to minimize sensitivity to extraneous loads. Moment compensated load cells are designed to counteract the external forces or moments by using a configuration of strain gages and electronics that can detect and compensate for these forces. The strain gages are arranged in a way that allows the load cell to measure the force applied to it in multiple directions, and the electronics can then use this information to calculate the impact of external forces and moments on the measurement.