Tag Archive for: deformation

Elasticity 101
Interface's Elasticity 101 details the importance of Hooke's Law of Physics. In a load cell, we want a material with a very predictable stiffness. If the material permanently deforms or creeps, the deformation value won't return to zero, and your measurements will be inaccurate. A load cell is essentially a mechanical transducer that converts mechanical force into elastic potential energy, which we then capture as data. Understanding how your sensor bends is the first step toward mastering precision force measurement. Learn more in Interface's ForceEDU 101 Series.

Core Measurement Fundamentals of Force, Stress, and Strain
Understanding differences in measuring force, stress, and strain, and how Interface's load cells accurately measure changes in objects, will help you better prepare to maximize the potential of your force measurement solutions for critical applications.

Resistance Output Versus Rated Output
Rated Output (RO) is the dynamic electrical signal that directly represents the applied mechanical force. Resistance Output is a static electrical characteristic of the load cell's internal circuitry. When you are performing force measurements, you are primarily interested in the Rated Output. This value, in conjunction with your excitation voltage, enables you to accurately convert the measured millivolt signal into engineering units of force in lbf or Newtons. Discover how load cells work at the ultimate force measurement resource hub, Interface ForceEDU.