A testing laboratory was looking to replace two single axis load cells used in their friction testing machine with one sensor that could measure force on the x, y, and z axis simultaneously.
A testing laboratory was looking to replace two single axis load cells used in their friction testing machine with one sensor that could measure force on the x, y, and z axis simultaneously.
Interface Solution
An Interface Model 3A60 3-Axis load cell was installed on their existing machine with an Interface BX3-HD44-CAN 3-Channel CANbus AND USB Strain Gage Amplifier hooked directly to a PC laptop to monitor and log the data in real time.
Results
The testing laboratory was able to simplify their sensor set-up and improve their data collection, creating more value for their end customer.
Materials
3A60 3-Axis Load Cell
BX3-HD44-CAN 3-Channel CANbus AND USB Strain Gage Amplifier
BlueDAQ software
Appropriate cabling
How it Works
The 3-Axis load cell is installed between the arm of the friction testing machine and the test specimen.
The BX3-HD44-CAN is installed between the 3-Axis load cell and the PC laptop.
Weights are placed on the top of the arm to create a down force.
The machine arm drags the test specimen across the material resting on the bed.
The 3-Axis load cell measures the forward/back force (x), side to side force (y) and down force (z) being applied to the test specimen.
The sensor’s output is fed to the BX3-HD44-CAN and to the PC laptop where it is displayed using the included software.