Interface suggests using their Interface Mini™ products such as the SSMF Fatigue Rated S-Type Load Cells. Two of these S-type load cells can be attached on either end of the bike’s handlebar stem, where it will measure the forces applied as the handlebar undergoes its fatigue test. Results can be measured, logged, and graphed with the SI-USB Universal Serial Bus Dual Channel PC Interface Module.