Solution
Tire Force and Moment
A tire production company wants to put their tires under a stress test in order to research the dynamic control capabilities of their tires.
A tire production company wants to put their tires under a stress test. They want to research the dynamic control capabilities of their tires. They want to measure both the torque and lateral force of the tire.
Interface suggests using the AT105 Contactless Force/Torque Transducer to measure both the lateral force and torque of the tired being tested. Torque and force results can be displayed and graphed when connected to theSI-USB4 4 Channel USB Interface Module.
After conducting a stress test on their tires, the tire production company was able to record and log the measurements of the torque and lateral forces implemented on their tires.