Tag Archive for: SMT

Tips for Properly Installing S-Type Load Cells
S-type load cell installation success hinges on protecting the sensor's gauged area from extraneous mechanical forces during setup. Interface provides installation tips, a setup video, and instructions. By ensuring that all tightening torque is applied to a single end, maintaining a minimum thread-depth engagement of one diameter, locking the threads to a shoulder or jam nut, and using high-grade hardware for loads exceeding the sensor’s capacity, you eliminate the leading causes of failure. Proper installation protects the load cell's calibration integrity, longevity, and safety across applications.

2025 Recap of Trending Interface Products
Explore Interface’s 2025 Product Recap to see the most popular load cells and torque transducers driving trends in advanced analytics, test lab upgrades, structural and fatigue testing, robotics, digital instrumentation, and miniaturization. By no surprise, Interface's 1200 LowProfile Load Cell remains in the number one spot for load cells. S-types and beams took the top spots and trends toward multi-axis sensors saw a rise in 3-Axis and 6-Axis sensors and systems.

Key Considerations for Overload Protection in Load Cells
Overload significantly threatens the accuracy, longevity, and safety of force measurement systems. An overload occurs when the force exerted on a load cell surpasses its designated capacity limit. Discover how Interface load cells incorporate innovative features to reduce the risks associated with overloading. Interface offers a number of standard LowProfile and Mini load cells with overload protection.

How Does Load Cell Overload Detection Work?
Load cell overload occurs when the force applied to a load cell exceeds its rated capacity. Load cells are designed to operate within specific load limits. Overload detection is essential to protect these costly and sensitive devices from damage and ensure the longevity and reliability of the sensors. Without proper overload protection, these sensors can be compromised, leading to inaccurate readings or permanent damage.

Understanding and Preventing Load Cell Overload
Interface offers patented overload protection for load cells. Overload detection is crucial for maintaining load cell accuracy. Properly detecting and handling overload conditions can prevent permanent damage and ensure the sensor's longevity. By understanding the signs of overload, managing impact loads, and employing preventive measures, users can maintain the integrity of their measurement systems. Regular maintenance and proper design considerations are vital to avoiding the detrimental effects of overload and ensuring accurate, long-term performance of load cells.