Solution
MDPS Testing
A car manufacturer wants to test the power steering for their vehicles. They want to test the linkage tension and compression between the rack and pinion.

A car manufacturer wants to test the power steering for their vehicles. They want to test the linkage tension and compression between the rack and pinion.
On a test frame, Interface’s 1200 Standard Precision LowProfile™ Load Cell is installed at the end of the rack and pinion actuator. As the wheel is turned, the load cell tests the push and pull forces. Force measurements can be displayed in real time using the highly accurate 9870 High-Speed High Performance TEDS Ready Indicator.
Interface’s 1200 Standard Precision LowProfile™ Load Cell successfully measured the tension and compression between the rack and pinion of the customer’s MDPS system.