Interface suggests installing Pillow Block Load Beam at both ends of the bottom roller to measure the forces being applied. The forces are measured when connected to WTS-AM-1E Wireless Strain Bridge Transmitter Module. The data is then transmitted wirelessly to the WTS-BS-6 Wireless Telemetry Dongle Base Station and the WTS-HK-S Next-Generation Wireless Handheld, where data can be displayed, graphed, and logged on the customer’s PC or laptop.