Interface’s WMC Sealed Stainless Steel Miniature Load Cell can be installed within the golf tee, which would measure the golf balls pressure on the tee when loaded or unloaded. This load cell is electrically connected to the motor which initiates the cycle to release another ball onto the tee. Force measurements can be measured using the 9330 High Speed Data Logger when connected to the customer’s PC or laptop.