Solution
Crude Oil Weighing
A weighing system is needed to measure mass amounts of crude oil.
Four SSB Sealed Beam Load Cells
JB104SS Junction Box
480 Bidirectional Weight Indicator
Four SSB Sealed Beam Load Cells are secured to the bottom of a metal platform.
Barrels of crude oil are placed on the Interface’s industrial scale, where it was weighed on the metal platform.
The multiple SSB’s were wired together to a JB104SS Junction Box, which was then connected to the 480 Bidirectional Weight Indicator to measure the combined results of the four SSB Sealed Beam Load Cells.