Interface Launches Global G Series for International Markets
Interface has launched a new international Mini™ Load Cell product line, the Global G Series, under it’s new product brand the Global Standard® Force Measurement.
The new miniature load cells were developed to meet the increasing demand for Interface high-precision, accurate and reliable force measurement solutions designed and manufactured in the International System of Units (SI), commonly known as the metric system.
The G Series debuts with Interface’s most popular Mini™ load cells, enabling international customers to purchase these Global Standard Force Measurement products through the company’s large network of distributors exclusively outside of the United States.
“The Interface brand is well-known worldwide for representing the premium standard for precision force and torque solutions. As demand for our products grew globally, we received many requests for SI-based designs of our load cells. We listened to our customers and are proud to launch our first G Series products that are the most popular miniature load cells used in aerospace and defense, automotive, medical and industrial automation industries worldwide.” ,” Greg Adams, CEO, Interface
Interface is manufacturing the Interface G Series lineup in the Asia-Pacific region, to provide customers with a near market advantage and access to the best force measurement solutions available today. Manufacturing these products near demand shortens the time and cost for customers to receive quality Interface products. Every product in the G Series has passed a rigorous Interface quality and engineering testing and calibration protocol to meet the highest in accuracy and quality standards.
The first release of G Series products available today through our global distributor network include:
- GLBM Series Load Button Load Cells – The GLBM Series Load Button Load Cells are strain gage-based transducers with temperature compensation and excellent overall performance. This type provides a range of capacities up to 200kN with better than ±0.5% (full scale) non-linearity.
- GSMTM Series Mini™ S-Beam Load Cell – The GSMTM Series Miniature S-Type Load Cells are a bi-directional aluminum strain gage-based transducer with high performance and built-in temperature compensation. This design provides better than ±0.1% (full scale) non-linearity and includes overload protection in both tension and compression directions.
- GWMC Series Mini™ Threaded In-Line Load Cells (10kN – 50kN) -The GWMC Series Miniature Threaded In-Line Load Cells are strain gage-based transducers with temperature compensation and excellent overall performance. This type measures tensile and compressive loads up to 50kN with better than ±0.5% non-linearity.
- GWMC Series Mini™ Threaded In-Line Load Cells (200N – 5000N) – The GWMC Series Miniature Threaded In-Line Load Cells are strain gage-based transducers with temperature compensation and excellent overall performance. This type measures tensile and compressive loads up to 5000N with better than ±0.25% non-linearity.
For more information about Interface Global Standard G Series solutions and to watch for new products for international markets, please visit www.interfaceforceglobal.com. Interface G Series products are not available for purchase in the United States.