Tag Archive for: sensor

Non-Repeatability 101
Interface 101 defines non-repeatability as the maximum difference between sensor output readings when the exact same load is applied repeatedly under identical loading and environmental conditions. Using load cells, understanding non-repeatability, why it governs a test's practical resolution limit, and how to isolate it from external test-rig anomalies is essential to designing dependable test protocols and accurate analysis.

How Do Universal Testing Machines Use Load Cells?
Universal testing machines (UTMs) are essential for material qualification, structural research, and quality assurance. Interface load cells sit directly in series with the moving crosshead and the upper specimen grip of a UTM. A machine controller reads the load cell continuously within a closed feedback loop to regulate crosshead travel, maintain constant loading rates, or hold targeted force thresholds during stress relaxation evaluations. The transducer measures the specimen resistance as it deforms. The data acquisition system pairs this instantaneous force data with displacement data to measure elasticity, yield point, and ultimate tensile strength.

What Is the Difference Between Fatigue and Impact Testing?
Interface Tech Talk details why fatigue testing and impact testing are fundamentally different mechanical test methodologies that impose separate physical and electronic demands on measurement hardware. Learn about application differences, load cell and sensor selection, and instrumentation requirements for each type of test.

Interface Data Sheet 101
Interface Data Sheet 101 reviews what to expect from our technical product data sheets. Consider data sheets as a technical roadmap of mechanical and electrical performance information. Interface data sheets include features, a reference image, performance specs, and drawings. The characteristics defined on a product data sheet are used to distinguish successful validation from a system failure by highlighting the individual model's specifications, dimensions, diagrams, characteristics, connectors, and wiring, when applicable.

Elasticity 101
Interface's Elasticity 101 details the importance of Hooke's Law of Physics. In a load cell, we want a material with a very predictable stiffness. If the material permanently deforms or creeps, the deformation value won't return to zero, and your measurements will be inaccurate. A load cell is essentially a mechanical transducer that converts mechanical force into elastic potential energy, which we then capture as data. Understanding how your sensor bends is the first step toward mastering precision force measurement. Learn more in Interface's ForceEDU 101 Series.

Interface New Products Releases in Winter 2025
Interface's new product releases include calibration and lab testing tools, a new multi-axis sensor, new instrumentation, and additions to Interface Complete Systems. Test and measurement is moving toward high-velocity data, advanced analytics, digital protocols, and continuous feedback to support automation, robotics, miniaturized product designs, and innovation in the test lab. These new products support these trends.

X-Y-Z Robots and Multi-Axis Sensors are Advancing Automation
X-Y-Z robots offer exceptional mechanical precision and rigidity for movement, and Interface multi-axis load cells provide real-time sensory input about force and torque. The powerful combination of the inherent mechanical precision and rigidity of X-Y-Z robots with the tactile intelligence provided by load cells represents a significant leap forward in industrial automation.

Connectors 101
Interface connectors are the critical link that physically and electrically connects a sensor's cable end to a corresponding receptacle on the instrumentation device. When selecting a cable for your test and measurement application, always consider the connector type at both ends to ensure compatibility and optimal performance. Use Interface guides to make the right connection between your load cell and data acquisition system.

Unveiling Interface Top Products of 2024
Interface load cells, torque transducers, and instrumentation play an integral role in pushing the boundaries of scientific discovery, optimizing industrial processes, and ensuring the safety and performance of countless products. Learn about the products that topped the charts in 2024 and what product families and standout individual products sparked the most interest.