Solution
Golf Ball Tee
A customer wants to ensure their golf ball automatic tee mechanism is working.

A customer wants to ensure their golf ball automatic tee mechanism is working. They need a system that will sense the presence of a golf ball, which will trigger and automatically dispense new golf ball to the tee.
Interface’s WMC Sealed Stainless Steel Miniature Load Cell can be installed within the golf tee, which would measure the golf balls pressure on the tee when loaded or unloaded. This load cell is electrically connected to the motor which initiates the cycle to release another ball onto the tee. Force measurements can be measured using the 9330 High Speed Data Logger when connected to the customer’s PC or laptop.
With Interface’s products, the customer was provided a force solution that was able to measure the presence of a golf ball on their auto-tee machine.