Solution


Package Drop Tester

A package drop test is an experiment of the falls that a package carrying goods experiences during shipping and handling.


PackageDropTest Graphic

Summary

  • Customer Need / Challenge

    A package drop test is an experiment of the falls that a package carrying goods experiences during shipping and handling. During the test, a full package will be dropped in various ways in order to find any weaknesses which can then be addressed. A force system is needed to help create the package drop test environment.

  • Interface Solution

    Four of Interface’s SSB Sealed Beam Load Cells are mounted to each corner of the of the tester’s platform. A package is dropped, and the SSB’s are connected to the JB104SS 4-Channel Stainless Steel Junction Box to sum the forces. The junction box is then connected to the WTS-AM-1F Fast Wireless Strain Bridge Transmitter Module. Data is wirelessly transmitted to the WTS-BS-4 USB Base Station connected customer’s computer, where it is displayed, logged, and graphed with supplied Log100 software.

  • Results

    Interface’s SSB Load Beam Load Cells successfully measured and monitored the force of the customer’s package drop tester experiment.

Materials


  • Four SSB Sealed Beam Load Cells

  • JB104SS 4-Channel Stainless Steel Junction Box

  • WTS-AM-1F Fast Wireless Strain Bridge Transmitter Module

  • WTS-BS-4 Wireless Base Station with Log100 Software

  • Customer PC

How it Works


  1. Four of Interface’s SSB Sealed Beam Load Cells are mounted to each corner of the of the tester’s platform.

  2. When a package is dropped, the SSB’s are connected to the JB104SS 4-Channel Stainless Steel Junction Box to sum the forces. The junction box is then connected to the WTS-AM-1F Fast Wireless Strain Bridge Transmitter Module.

  3. Data is wirelessly transmitted to the WTS-BS-4 USB Base Station which is connected to the customer’s computer, where it is displayed, logged, and graphed with supplied Log100 software.

Download PDF