Solution
Mining Truck Scale
Mining trucks carry many different loads such as ore, coal, and minerals. A weighing system is needed to ensure the mining truck is not overloaded during transportation.

WTS 1200 Standard Precision LowProfile™ Wireless Load Cells
WTS-BS-4 USB Industrial Base Station
WTS-LD2 Wireless Large LED Display
WTS Toolkit and Log100 Software
Customer PC or Laptop
Multiple WTS 1200 Standard Precision LowProfile™ Wireless Load Cells are installed and mounted to the bottom of the truck weighing scale.
The load cells collect the force measurements and sum the total weight of the mining truck carrying a heavy load.
The data is transmitted to the customer’s laptop through the WTS-BS-4 USB Industrial Base Station using the Log100 Software. The sum weight data can be logged, graphed, and sent to the cloud using the supplied software.
The WTS-LD2 Wireless Large LED Display can also display the weight inside of the vehicle for the driver to see in real time.