Solution


Gantry Crane Weighing

Gantry cranes are used for a number of mobile and lifting applications within industrial or construction environments. A weighing system is needed to see if the gantry crane can handle lifting heavy containers or loads, preventing crane failure or accidents.


GantryCraneWeighing Graphic

Summary

  • Customer Need / Challenge

    Gantry cranes are used for a number of mobile and lifting applications within industrial or construction environments. A weighing system is needed to see if the gantry crane can handle lifting heavy containers or loads, preventing crane failure or accidents.

  • Interface Solution

    Interface’s WTSLP Wireless Stainless Steel Load Pins can be installed into the corners of the lifting mechanism of the gantry crane, where heavy loaded containers are lifted and moved. The force results are then wireless transmitted to both the WTS-HK-S Next-Generation Wireless Handheld, or directly to the customer’s PC with the WTS-BS-6 Wireless Telemetry Dongle Base Station.

  • Results

    The customer was able to monitor the loads lifted from their gantry crane with Interface’s Wireless Telemetry System, and determine whether or not their gantry crane was able to handle lifting heavy loads.

Materials


  • Four WTSLP Wireless Stainless Steel Load Pin
  • WTS-HK-S Next-Generation Wireless Handheld
  • WTS-BS-6 Wireless Telemetry Dongle Base Station
  • Supplied Log100 software
  • Customer PC

How it Works


  1. The four WTSLP Wireless Stainless Steel Load Pin are installed at the our corners of the lifting mechanism of the gantry crane. A heavy load or container is lifted.
  2. The WTSLP’s wirelessly transmits the force data results to WTS-HK-S Next-Generation Wireless Handheld, or directly to the customer’s PC with the WTS-BS-6 Wireless Telemetry Dongle Base Station. Data can be logged, graphed, and recorded with supplied Log100 software.

Download PDF