Solution
Continuum Robot Testing
A continuum robot is a robotic arm that has a continuously curving design, that acts similarly to the trunk of an elephant. It is very maneuverable, and is used for tedious applications such as robotic surgery.

6A40 6-Axis Standard Capacity Load Cell
BX8-AS BlueDAQ Series Data Acquisition System with supplied software
Customer computer
Customer continuum arm undergoing test
The 6A40 6-Axis Standard Capacity Load Cell is installed at the base of the continuum arm.
The BX8-AS BlueDAQ Series Data Acquisition System is connected to the 6A40 6-Axis load cell and the customer’s PC Laptop.
As the continuum robotic arm undergoes a functionality test the load cell measures forces in all axes (Fx, Fy, Fz, Mx, My, Mz). The BX8-AS displays, logs, and graphs all measurements onto the customer’s computer.