Solution
Aerial Arts Rig
An aerialist needs to measure how heavy they are on their aerial arts rig to ensure it can hold them during their performance. They want to ensure they rig will be stable, and will not reach the load limit.
An aerialist needs to measure how heavy they are on their aerial arts rig to ensure it can hold them during their performance. They want to ensure they rig will be stable, and will not reach the load limit.
Interface’s 6A80 Series 6-Axis Standard Capacity Load Cell is fitted with a rod end bearing and attached to the top aerial rig with a type of swivel mount. It is also connected to the BX8-HD44 BlueDAQ Series Data Acquisition System. The aerialist performer hangs from the rig, and their weight load results are fed to the BX8-HD44 BlueDAQ Series Data Acquisition System with supplied BlueDAQ software and to the connected laptop where it is displayed with included BlueDAQ software.
The aerialist was able to determine if their aerial arts rig was able to hold their weight during a performance with Interface’s force measurement system.